Tool/software:
UFS is present on the J784S4EVM. How can one use it instead of eMMC to host rootfs and use that to boot to Linux command prompt.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
UFS is present on the J784S4EVM. How can one use it instead of eMMC to host rootfs and use that to boot to Linux command prompt.
Hi,
Steps below:
root@j721e-evm:~# fdisk /dev/sdb Welcome to fdisk (util-linux 2.37.4). Changes will remain in memory only, until you decide to write them. Be careful before using the write command. The device contains 'ext4' signature and it will be removed by a write command. See fdisk(8) man page and --wipe option for more details. Device does not contain a recognized partition table. Created a new DOS disklabel with disk identifier 0x511d1827. Command (m for help): m Help: DOS (MBR) a toggle a bootable flag b edit nested BSD disklabel c toggle the dos compatibility flag Generic d delete a partition F list free unpartitioned space l list known partition types n add a new partition p print the partition table t change a partition type v verify the partition table i print information about a partition Misc m print this menu u change display/entry units x extra functionality (experts only) Script I load disk layout from sfdisk script file O dump disk layout to sfdisk script file Save & Exit w write table to disk and exit q quit without saving changes Create a new label g create a new empty GPT partition table G create a new empty SGI (IRIX) partition table o create a new empty DOS partition table s create a new empty Sun partition table Command (m for help): p Disk /dev/sdb: 29.79 GiB, 31981568000 bytes, 7808000 sectors Disk model: THGAF8G8T23BAILB Units: sectors of 1 * 4096 = 4096 bytes Sector size (logical/physical): 4096 bytes / 4096 bytes I/O size (minimum/optimal): 65536 bytes / 65536 bytes Disklabel type: dos Disk identifier: 0x511d1827 Command (m for help): n Partition type p primary (0 primary, 0 extended, 4 free) e extended (container for logical partitions) Select (default p): p Partition number (1-4, default 1): First sector (256-7807999, default 256): [ 45.123255] kauditd_printk_skb: 3 callbacks suppressed [ 45.123262] audit: type=1334 audit(1715059470.964:17): prog-id=12 op=UNLOAD [ 45.135361] audit: type=1334 audit(1715059470.964:18): prog-id=11 op=UNLOAD [ 45.593936] systemd-journald[165]: Time jumped backwards, rotating. Last sector, +/-sectors or +/-size{K,M,G,T,P} (256-7807999, default 7807999): Created a new partition 1 of type 'Linux' and of size 29.8 GiB. Command (m for help): p^H^H^H Disk /dev/sdb: 29.79 GiB, 31981568000 bytes, 7808000 sectors Disk model: THGAF8G8T23BAILB Units: sectors of 1 * 4096 = 4096 bytes Sector size (logical/physical): 4096 bytes / 4096 bytes I/O size (minimum/optimal): 65536 bytes / 65536 bytes Disklabel type: dos Disk identifier: 0x511d1827 Device Boot Start End Sectors Size Id Type /dev/sdb1 256 7807999 7807744 29.8G 83 Linux Command (m for help): m Help: DOS (MBR) a toggle a bootable flag b edit nested BSD disklabel c toggle the dos compatibility flag Generic d delete a partition F list free unpartitioned space l list known partition types n add a new partition p print the partition table t change a partition type v verify the partition table i print information about a partition Misc m print this menu u change display/entry units x extra functionality (experts only) Script I load disk layout from sfdisk script file O dump disk layout to sfdisk script file Save & Exit w write table to disk and exit q quit without saving changes Create a new label g create a new empty GPT partition table G create a new empty SGI (IRIX) partition table o create a new empty DOS partition table s create a new empty Sun partition table Command (m for help): w The partition table has been altered. Calling ioctl() to re-read partition table. [ 55.711671] sdb: sdb1 Syncing disks. root@j721e-evm:~# lsblk -l NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS sda 8:0 0 32M 0 disk sda1 8:1 0 31M 0 part sdb 8:16 0 29.8G 0 disk sdb1 8:17 0 29.8G 0 part mtdblock0 31:0 0 512K 0 disk mtdblock1 31:1 0 2M 0 disk mtdblock2 31:2 0 4M 0 disk mtdblock3 31:3 0 128K 0 disk mtdblock4 31:4 0 128K 0 disk mtdblock5 31:5 0 1M 0 disk mtdblock6 31:6 0 55.8M 0 disk mtdblock7 31:7 0 128K 0 disk mtdblock8 31:8 0 512K 0 disk mtdblock9 31:9 0 2M 0 disk mtdblock10 31:10 0 4M 0 disk mtdblock11 31:11 0 128K 0 disk mtdblock12 31:12 0 128K 0 disk mtdblock13 31:13 0 1M 0 disk mtdblock14 31:14 0 55.8M 0 disk mtdblock15 31:15 0 128K 0 disk mmcblk0 179:0 0 14.8G 0 disk mmcblk0p1 179:1 0 14.8G 0 part mmcblk0boot0 179:32 0 31.5M 1 disk mmcblk0boot1 179:64 0 31.5M 1 disk mmcblk1 179:96 0 14.8G 0 disk mmcblk1p1 179:97 0 128M 0 part /boot mmcblk1p2 179:98 0 7.4G 0 part / root@j721e-evm:~# sudo mkfs -t ext4 /dev/sdb1 mke2fs 1.46.5 (30-Dec-2021) Creating filesystem with 7807744 4k blocks and 1954064 inodes Filesystem UUID: e1bac28e-f771-40a4-b06e-71f93217ad3e Superblock backups stored on blocks: 32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208, 4096000 Allocating group tables: done Writing inode tables: done Creating journal (32768 blocks): done Writing superblocks and filesystem accounting information: done root@j721e-evm:~# sudo mkfs -t vfat /dev/sda1 mkfs.fat 4.2 (2021-01-31) root@j721e-evm:~# lsblk -f NAME FSTYPE FSVER LABEL UUID FSAVAIL FSUSE% MOUNTPOINTS sda `-sda1 vfat BCF8-546B sdb `-sdb1 ext4 e1bac28e-f771-40a4-b06e-71f93217ad3e 27.6G 0% /run/media/sdb1
diff --git a/arch/arm64/configs/defconfig b/arch/arm64/configs/defconfig index c59d34af1..8f613d311 100644 --- a/arch/arm64/configs/defconfig +++ b/arch/arm64/configs/defconfig CONFIG_SCSI_UFS_QCOM=m CONFIG_SCSI_UFS_HISI=y CONFIG_SCSI_UFS_RENESAS=m -CONFIG_SCSI_UFS_TI_J721E=m +CONFIG_SCSI_UFS_TI_J721E=y
mkdir /mnt/ufs mkdir /mnt/sd cp -r /mnt/sd/* /mnt/ufs sync umount /mnt/*
setenv bootargs console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 root=/dev/sdb1 rootwait setenv bootcmd "ufs init; scsi scan; ext4load scsi 1 0x82000000 boot/Image; ext4load scsi 1 0x81200000 boot/dtb/ti/k3-j784s4-evm.dtb; booti 0x82000000 - 0x81200000" boot