Part Number: SK-AM69
Other Parts Discussed in Thread: J721EXENETXPANEVM, , AM69
Tool/software:
Hello,
we want to use the J721EXENETXPANEVM Quad ETH expansion card with our SK-AM69 dev kit. We know this combination is not yet suppored, but according to another thread it should not be a big problem. Detailed schematic can be found here.
Because the SK-AM69 does not have a clock generator, we want to use the one on the Quad ETH expansion card (part U4). Resistors R26 and R27 are removed, resistors R23 and D24 are soldered (as jumpers). The CDCI_I2C_SEL signal is set to '1' when Linux boots. And now the problems:
- The clock generator has an I2C address of 0x76, which is different from the schematic. It appears that the last bit of the address in EEPROM Page 1 is factory programmed by TI to '0'. Is that correct?
- I2C communication does not work at startup (bus errors). We have to manually reset the clock generator with pin 8 (RESET/SYNC). It is odd, because in the schematic it is permanently connected to '1' via a pull-up resistor and is not controlled, so a reset does not seem to be necessary. Can you clarify this behavior?
- After manual reset registers can be read/write wtihout problem. However, there is no signal on the clock outputs. List of all registers are listed on the end. All registers are loaded from the EEPROM, we do not write anything yet. Flag 'nvmbusy' in register STATUS1 is suspicious.
Can you try to reproduce this behavior in your setup or give me some tips what is wrong with our setup?
And one more question. AM69 SERDES2 REFCLK is connected to the Quad Eth expansion card by default. Can we use REFCLK as a clock source for the PHY on the expansion card if the option with the clock generator fails?
R70 0x00460000
R69 0x00450000
R68 0x00440000
R67 0x00430020
R66 0x00420000
R65 0x00410F34
R64 0x0040000D
R63 0x003F0210
R62 0x003E4210
R61 0x003D1000
R60 0x003C0010
R59 0x003B0009
R58 0x003A0008
R57 0x00390A65
R56 0x00380405
R55 0x00370004
R54 0x00360000
R53 0x00358000
R52 0x00340008
R51 0x00330A65
R50 0x00320405
R49 0x00310004
R48 0x00300000
R47 0x002F8000
R46 0x002E0008
R45 0x002D0A65
R44 0x002C0405
R43 0x002B0004
R42 0x002A0000
R41 0x00298000
R40 0x00280008
R39 0x00270A65
R38 0x00260405
R37 0x00250004
R36 0x00240000
R35 0x00238000
R34 0x00220050
R33 0x00210007
R32 0x00200000
R31 0x001F1E72
R30 0x001E5140
R29 0x001D400A
R28 0x001C0000
R27 0x001B0000
R26 0x001A0718
R25 0x001902C2
R24 0x00180601
R23 0x00170593
R22 0x00160800
R21 0x00150000
R20 0x00140001
R19 0x00130000
R18 0x0012400A
R17 0x001126C4
R16 0x0010921F
R15 0x000FA037
R14 0x000E0000
R13 0x000D0000
R12 0x000C0000
R11 0x000B0000
R10 0x000A0000
R9 0x00090000
R8 0x00080001
R7 0x00070E10
R6 0x000619CA
R5 0x00050028
R4 0x00040055
R3 0x00030000
R2 0x00020053
R1 0x00016882
R0 0x00000000