This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM620-Q1: Connect SRAM to GPMC

Part Number: AM620-Q1


Tool/software:

Hi TI Team,

I would like to avoid LPDDR4 memory because of cost. 

Is it possible to connect a standard 16-bit SRAM to the GPMC?

Can you recommend any p/n?

What is the maximum addressing size?

Voltage interface would be 1.8V?

Could you please provide feedback to the above questions.

BR FM