Part Number: AM6442
Tool/software:
Hello,
I am using mcu_plus_sdk_am64x_09_01_00_41 and have written code to measure GPIO write and read times.
The R5F core clock is set to 800 MHz, and the GPIO peripheral clock (GPIO0_VBUS_FICLK) is set to 125 MHz.
Below is the code flashed to the R5F core. The waveforms were observed on an oscilloscope:
gpioBaseAddr = (uint32_t) AddrTranslateP_getLocalAddr(GPIO_LED_BASE_ADDR);
pinNum = GPIO_LED_PIN;
GPIO_setDirMode(gpioBaseAddr, pinNum, GPIO_LED_DIR);
gpioBaseAddr1 = (uint32_t) AddrTranslateP_getLocalAddr(OUTPUT_GPIO_BASE_ADDR);
pinNum1 = OUTPUT_GPIO_PIN;
GPIO_setDirMode(gpioBaseAddr1, pinNum1, OUTPUT_GPIO_DIR);
uint32_t regIndex1, regVal1;
volatile CSL_GpioRegs* hGpio = (volatile CSL_GpioRegs*)((uintptr_t) gpioBaseAddr1);
regIndex1 = GPIO_GET_REG_INDEX(pinNum1);
regVal1 = GPIO_GET_BIT_MASK(pinNum1);
uint32_t regIndex, regVal;
volatile CSL_GpioRegs* hGpio1 = (volatile CSL_GpioRegs*)((uintptr_t) gpioBaseAddr);
regIndex = GPIO_GET_REG_INDEX(pinNum);
regVal = GPIO_GET_BIT_MASK(pinNum);
while(1)
{
CSL_REG32_WR(&hGpio->BANK_REGISTERS[regIndex1].SET_DATA, regVal1);
CSL_REG32_WR(&hGpio->BANK_REGISTERS[regIndex1].CLR_DATA, regVal1);
CSL_FEXTR(hGpio1->BANK_REGISTERS[regIndex].IN_DATA, regVal, regVal);
CSL_REG32_WR(&hGpio->BANK_REGISTERS[regIndex1].SET_DATA, regVal1);
CSL_REG32_WR(&hGpio->BANK_REGISTERS[regIndex1].CLR_DATA, regVal1);
}
From the waveforms, we observed the following timings:
- GPIO High time: ~210 ns
- GPIO Low time: ~210 ns
- GPIO Read time: ~210 ns
Could you please confirm if these timings are correct?
Additionally, I would like to know if it is possible to increase the GPIO peripheral clock frequency beyond 125 MHz to achieve a time lower than 210 ns. If it is possible to increase the peripheral clock frequency, what are the steps to change it?

Can we increase the PLL0_hsdiv0 value more than 500MHz? And what is the maximum value of PLL0_hsdiv0 is allowed?
Thank you,
Pratibha