This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: Cannot output image data to HDMI display

Expert 2690 points
Part Number: AM4378
Other Parts Discussed in Thread: TFP410,

Tool/software:

Hi All,

My customer is unable to output image data to an HDMI display via AM4378 and TFP410 HDMI transmitter.

Is there any reference material that can help us?
If you have any information on how to set up the device tree, drivers, etc.

The situation is as follows.
・Communication with TFP410 is working via AM4378 and I2C communication.
・HDMI display is connected to TFP410 via HDMI connector, HTPLG of TFP410 is Hi, and TFP410 seems to be detecting the display.
・Possibly the DSS of the MPU is not working from AM4378 (IDCK+, VSYNC, HSYNC, and DE signals are always Low).

Best Regards,

ito