Other Parts Discussed in Thread: AM62L
Tool/software:
HI TI experts,
Could you provide recommendations on CAP_VDDSx, cap value and effect of the capacitor not mounted or shorted.
HI Board designers,
Recommendations on CAP_VDDSx value
The LDO specification is 0.8uF to 1.5uF. The capacitor should be within this range, considering bias, degradation over time etc.
Q. With a 6.3V cap selected, considering the DC effect and other degradation, the cap value could go down to 0.7 uF. Higher cap value may call for using a 0402 cap and that could have an effect on the layout.
Does the capacitance depend on number of IOs used for the specific IO supply rail and the IOs current source/sink or irrespective of the IO usage, the capacitance is required.
https://www.kyocera-avx.com/docs/techinfo/CeramicCapacitors/mlcc-dc-bias-characteristics.pdf
The cap value is independent of IO count and activity. It is required for stability of the LDO to generate BIAS supply. Any value beyond this specified range could make BIAS generator unstable resulting in over voltage stress.
Additional Guidelines
Select cap with less the 1 ohm ESR
Ensure the PCB loop inductance is < 2.5 nH
Use smallest possible (0201 or greater) package to minimize loop inductance
Refer SoC Data sheet
Regards,
Sreenivasa
HI Board designers,
CAP_VDDSx voltage
It is not a fixed voltage. When the respective VDDSHV is operating at 1.8V, the pin should have the same potential as the VDDSHV source.
When the respective VDDSHV is operating at 3.3V, it should have a potential that track to ½ of the VDDSHV source.
When VDDSHV is ramping to 3.3V the LDO output will track VDDSHV until it gets up to about 2.4V. This is when bias supply circuit changes from what I call switch mode to LDO mode. At this point it begin to track ½ VDDSHV. I suspect the output capacitance will hold the 2.4V potential for a period of time before the IO bias circuits draw enough current to discharge the capacitor back down to the ½ VDDSHV potential.
I would expect a similar thing to happen as the VDDSHV decays. When VDDSHV drops below 2.4V the bias supply circuit will switch back to switch mode, where the potential of VDDSHV is applied to the capacitor.
The CAP_VDDSn is optional when the IO group supply VDDSHVx is connected to 1.8V. When connected to 3.3V, the voltage to be considered for derating is the steady state DC output which is VDDSHVx/2.
Regards,
Sreenivasa
HI Board designers,
Effect of the CAP_VDDSx on the SOC performance
The capacitor is connected to the output of an internal LDO. The LDO will not function correctly if the capacitor is not connected to this pin or if this pin is shorted to ground. The LDO powers circuits in each IO buffer associated with the respective bank of IOs. The IO buffers will not operate as expected if the LDO is not operating as expected. If the LDO is not operating properly the IO buffer circuits may be permanently damaged. Any SOC that has been exposed to a condition that prevents the LDO from operating as expected should be removed, discarded, and replaced with a new unit.
Regards,
Sreenivasa
HI Board designers,
Updates for AM62L
AM62L supports 1.8V fixed voltage IOs and Dual-voltage fixed or dynamically switched IOs
Caps are required for Dual-voltage IO supply for IO groups
CAP_VDDS_GENERAL1 CAP External capacitor connection for GENERAL1 IO group
CAP_VDDS_GPMC External capacitor connection for GPMC IO group
CAP_VDDS_MMC0 External capacitor connection for MMC0 IO group
CAP_VDDS_MMC1 External capacitor connection for MMC1 IO group
CAP_VDDS_MMC2 External capacitor connection for MMC2 IO group
This pin must always be connected via a 6.3V or greater, 0.8uF to 1.5μF capacitor to VSS if the respective VDDSHVx pin is ever operated at 3.3V IO supply. The capacitor selected must provide a capacitance within the defined range after it has been derated for DC-bias, operating temperature, and aging effects. There are three connection options if the respective VDDSHVx pin is only operated at 1.8V. The pin can be connected to the same decoupling capacitor that is required for 3.3V operation, it can be left unconnected, or it can be connected to the same 1.8V power source as the respective VDDSHVx pin.
AM62L supports integrated LDO for powering the SD card interface
CAP_VDDSHV_MMC External capacitor connection for SDIO_LDO
This pin must always be connected via a 6.3V or greater, 3.3μF ±20% capacitor to VSS when the SDIO_LDO is being used to source VDDSHV3 or VDDSHV4. The capacitor selected must provide a capacitance within the defined range after it has been derated for DC-bias, operating temperature, and aging effects. Otherwise, this pin may be connected directly to VSS when the VDDA_3P3_SDIO pin is also connected directly to VSS.
Regards,
Sreenivasa