Other Parts Discussed in Thread: FFTLIB
Tool/software:
Hi
I have a test application developed for computing the FFT for our custom raw data and the linker file for our test application is as follows,
Processor : J784s4_evm
Core : C7x_1
Here the memory address for L1 and L2 Ram is taken from the system_memory_map from the vision_apps.
In FFTLib lnk.cmd "ti-processor-sdk-rtos-j784s4-evm-09_02_00_05\fftlib_09_02_00_04\cmake\linkers\C7120\lnk.cmd" , the memory address given for L1 and L2 looks different , can you please comment on these addresses where these are used in the FFT library because I am facing issue while booting this test application from linux system which is clashing some how with the memory