Part Number: SK-AM62P-LP
Tool/software:
Hello TI,
We are using am62p-lp and trying to connect with xds debugger trough micro usb connector(JTAG).
while launching the target configurations i am getting error reporting as below.This is the test connection log.
[Start: Texas Instruments XDS110 USB Debug Probe_0] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ /home/svaya_22/.ti/ccs1281/0/0/BrdDat/testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100/110/510 class product. This utility will load the adapter 'libjioxds110.so'. The library build date was 'Sep 26 2024'. The library build time was '10:06:50'. The library package version is '20.0.0.3178'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-260' (0xfffffefc). The title is 'SC_ERR_XDS110_OPEN'. The explanation is: An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. [End: Texas Instruments XDS110 USB Debug Probe_0]