This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VM-Q1: MDIO change in SR2.0

Part Number: TDA4VM-Q1
Other Parts Discussed in Thread: TDA4VM

Tool/software:

Hi Expert,

My customer Motovis report an issue about ethernet link down issue, customer have catch the MDIO using the Logic analysis, they find there is some difference between B version (SR1.1) and C version (SR2.0). customer are using the same SW, and they actually only send the clause 22 protocol, and they can see only clause 22 in SR1.1 device, but in SR2.0, there is a lot of clause 45 you can see below screen shot. this difference cause customer line down, all SR2.0 board will link down so that the ethernet will work abnormal. need you help for this issue urgently; do you know any SW change need to be apply for this MDIO in GP device? or any difference between this? customer confirm this issue is related silicon version.

SDK version: SDK 8.4, GP Device

SR1.1:

SR2.0

0003.decoder--Bversion SR1.1 mdio.xlsx0003.decoder--C version SR2.0 mdio.csv

BR,

Biao