Part Number: TDA4VEN-Q1
Tool/software:
Hi , TI experts :
Because of limitation size of emmc BOOT#0 & BOOT#1 which is 4M , it's impossible that trying to using "fast boot" option in sbl_emmc_hlos boot mode , as the size of combined app is up to 21M.
So I tried to boot from emmc UDA partition .
- I partition the emmc UDA into BOOT in vfat and rootfs linux just like SDcard partition
- copy sbl_emmc_hlos.release.hs_fs.tiimage into BOOT as tiboot3.bin , and linux.appimage.hs_fs as app which in "fast boot " compile option
- firstly , boot from SDcard , enter the uboot cmd , configure the mmc :
```
mmc partconf 0 0 7 0
mmc bootbus 0 2 0 0
```
- switch bootpins from emmc RAW mode into emmc FS mode
Finally , there isn't any logs from uart after power on .
So , I would like to know any error in my steps or how can i boot from UDA partition in j722s .
SDK version : linux , rtos 10_00_00_08
Thank u very much
BR
stream