Tool/software:
Hi Team,
We are performing SI analysis of the connection I/F between TMS320C6748EZWT4 and DDR2.
Fail is occurring in Vix of Clock line during Fast/Typ condition.
The difference in the rise and fall times of the IBIS model on the DSP side may be a factor.
Is there any way to improve this crosspoint misalignment?
The following is the Clock line waveform under Fast conditions.
Because the P/N cross point is below the allowable voltage range Vix_min
It does not meet JEDEC's Vix requirements.
Therefore, the memory circuit may not function properly.