Part Number: SK-AM62A-LP
Tool/software:
Hi
I use ubuntu22.04 and the sdk is ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07-Linux-x86-Install.bin
I have three computer configurations, namely i7 8750H with 32GB RAM; i58265U RAM16G; i9 12900H RAM40G; The document states that the RAM should have 32GB or be configured with a swap. I have all configured a 32GB swap, but only I9 can complete the MACHINE=am62axx-evm bitbake tisdk-default-image.
1--why other configurations can not.
2-- When i use computer with i9 ,websocket and docker ce also cannot be downloaded.
Is there any good way to solve these problem.
thanks