Other Parts Discussed in Thread: AM62A7
Tool/software:
Hello TI experts,
We met issue about Partial-IO wake up source, MCU_CAN RX PIN working mode on TI platform.
Our environment is as following:
TI SDK BSP version: V09_00_02
Linux version: 6.1.80
We purchased TI AM62A7-SK-EVM and followed 3.2.2.12.5. Low Power Modes — Processor SDK AM62x Documentation to set MCU_CAN0 & MCU_CAN1 to be Partial-IO wake-up source.
It works, but the MCU_CAN RX PIN was kept about 0.6V and easily to be triggered by any high or low level changes on TI AM62A7-SK-EVM.
In general CAN PHY transceiver's action, MCU_CAN RX should be kept 3.3V and working to be low level for signal announcement.
When we connected the CAN PHY transceiver and MCU_CAN RX on TI AM62A7-SK-EVM.
And We do Partial-IO setiing then enter low power mode. The TI AM62A7-SK-EVM is waked up immediately.
The cause is that AM62A7 is triggerd by CAN PHY transceiver default 3.3V level...
To solve this issue.
Is there any way to set Partial-IO wake up source, MCU_CAN RX PIN to be trigger mode in low level trigger?