This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: USB Compliance Test Tools for AM4378 with Linux

Guru 13095 points
Part Number: AM4378


Tool/software:

Hi,

We are currently working on a project that requires performing a USB compliance test for the AM4378 device. According to the testing company, it is understood that device manufacturers may provide tools to support USB compliance testing. Could you confirm if TI offers any tools or guidance for performing USB compliance tests for the AM4378? 

Currently, the AM4378 is running on Linux. If there are any USB compliance test tools or utilities that can be used in a Linux environment, we would greatly appreciate it if you could share information regarding these tools or their setup.

Additionally, if there are any specific instructions or configurations for enabling USB test modes (such as test packets or other compliance-related features) on the AM4378 while using Linux, please let us know.

Thanks,

Conor