Part Number: AM67
Tool/software:
Hi
I want to check if this A24 pin used as GPIO or SDWP. How to configure this in SW, A24 is connected to PMIC.

Regards
Zekun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AM67 processor pin A24 can be either GPIO or SDWP. The various pin modes for each pin are defined in the data manual. If the pin is connected to PMIC, likely used as GPIO. Each LVCMOS pin has a pad configuration register (location also provided in data manual). From snip-it below, you can see the various pin modes supported (MUX MODE setting) and the pad config register (PADCONFIG145).