Tool/software:
Hello TI Team,
Our team is working on the AM625 project. The model used is AM6254, and the SDK version is 09.02.01.10. When we use the boot card made from the SD card image to boot the system, everything is normal. At this time, the AM625 is in Quad Core mode.
When we change the AM625 from Quad Core to Dual Core, recompile and overwrite the original Image and device tree. When the system is loading in the second half, the error shown in the figure occurs.
The following two pictures show the content I added to the file arch/arm64/boot/dts/ti/k3-am625-sk.dts.
The following is the entire log with errors.
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 13408 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Starting ATF on ARM64 core...
NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE: BL31: Built : 16:09:05, Feb 9 2024
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 1856 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
U-Boot 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SoC: AM62X SR1.0 GP
Model: Texas Instruments AM625 SK
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
DRAM: 2 GiB
Core: 72 devices, 32 uclasses, devicetree: separate
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In: serial
Out: serial
Err: serial
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
574 bytes read in 14 ms (40 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
## Error: "main_cpsw0_qsgmii_phyinit" not defined
19376640 bytes read in 221 ms (83.6 MiB/s)
58944 bytes read in 17 ms (3.3 MiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK
Working FDT set to 8feee000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.1.83-dirty (joey@linux-vm) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #2 SMP PREEMPT Tue Dec 31 11:30:34 CST 2024
[ 0.000000] Machine model: Texas Instruments AM625 SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
[ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009c7fffff]
[ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff]
[ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff]
[ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff]
[ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ff6fffff]
[ 0.000000] node 0: [mem 0x00000000ff700000-0x00000000fffeffff]
[ 0.000000] node 0: [mem 0x00000000ffff0000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: Embedded 20 pages/cpu s41064 r8192 d32664 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),98048k@32m(ospi.rootfs),256k@130816k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=01cc07ea-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1839356K/2097152K available (11712K kernel code, 1258K rwdata, 3816K rodata, 1984K init, 438K bss, 126724K reserved, 131072K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008593] Console: colour dummy device 80x25
[ 0.013209] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023892] pid_max: default: 32768 minimum: 301
[ 0.028669] LSM: Security Framework initializing
[ 0.033548] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.041133] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.051188] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.058647] cblist_init_generic: Setting shift to 1 and lim to 1.
[ 0.064957] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.072357] cblist_init_generic: Setting shift to 1 and lim to 1.
[ 0.078767] rcu: Hierarchical SRCU implementation.
[ 0.083679] rcu: Max phase no-delay instances is 1000.
[ 0.089334] Platform MSI: msi-controller@1820000 domain created
[ 0.095703] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.105123] EFI services will not be available.
[ 0.110010] smp: Bringing up secondary CPUs ...
[ 0.115414] Detected VIPT I-cache on CPU1
[ 0.115549] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[ 0.115571] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000
[ 0.115632] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.115773] smp: Brought up 1 node, 2 CPUs
[ 0.145172] SMP: Total of 2 processors activated.
[ 0.149984] CPU features: detected: 32-bit EL0 Support
[ 0.155257] CPU features: detected: CRC32 instructions
[ 0.160573] CPU: All CPU(s) started at EL2
[ 0.164762] alternatives: applying system-wide alternatives
[ 0.172534] devtmpfs: initialized
[ 0.185286] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.195315] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.208165] pinctrl core: initialized pinctrl subsystem
[ 0.214382] DMI not present or invalid.
[ 0.219079] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.226463] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.233887] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.241963] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.250172] audit: initializing netlink subsys (disabled)
[ 0.256020] audit: type=2000 audit(0.160:1): state=initialized audit_enabled=0 res=1
[ 0.256653] thermal_sys: Registered thermal governor 'step_wise'
[ 0.263961] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.270321] cpuidle: using governor menu
[ 0.281208] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.288208] ASID allocator initialised with 65536 entries
[ 0.304965] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[ 0.314471] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@f0000/pinctrl@a40000/cpsw-cpts
[ 0.325896] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[ 0.336854] KASLR disabled due to lack of seed
[ 0.348817] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.355802] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.362213] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.369152] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.375559] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.382498] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.388906] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.395847] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.404056] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[ 0.414913] iommu: Default domain type: Translated
[ 0.419927] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.426678] SCSI subsystem initialized
[ 0.430951] usbcore: registered new interface driver usbfs
[ 0.436606] usbcore: registered new interface driver hub
[ 0.442064] usbcore: registered new device driver usb
[ 0.447807] pps_core: LinuxPPS API ver. 1 registered
[ 0.452887] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.462240] PTP clock support registered
[ 0.466391] EDAC MC: Ver: 3.0.0
[ 0.470766] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[ 0.477935] FPGA manager framework
[ 0.481546] Advanced Linux Sound Architecture Driver Initialized.
[ 0.488854] clocksource: Switched to clocksource arch_sys_counter
[ 0.495405] VFS: Disk quotas dquot_6.6.0
[ 0.499476] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.513187] NET: Registered PF_INET protocol family
[ 0.518530] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.527897] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.536739] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.544678] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.552910] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.561045] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.567984] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.574920] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.582489] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.588817] RPC: Registered named UNIX socket transport module.
[ 0.594928] RPC: Registered udp transport module.
[ 0.599740] RPC: Registered tcp transport module.
[ 0.604548] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.611165] NET: Registered PF_XDP protocol family
[ 0.616087] PCI: CLS 0 bytes, default 64
[ 0.621102] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.631517] Initialise system trusted keyrings
[ 0.636407] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[ 0.647889] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.654630] NFS: Registering the id_resolver key type
[ 0.659855] Key type id_resolver registered
[ 0.664137] Key type id_legacy registered
[ 0.668294] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.675156] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.717541] Key type asymmetric registered
[ 0.721742] Asymmetric key parser 'x509' registered
[ 0.726801] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.734582] io scheduler mq-deadline registered
[ 0.739227] io scheduler kyber registered
[ 0.747352] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[ 0.753954] pinctrl-single f4000.pinctrl: 171 pins, size 684
[ 0.761666] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 0.774996] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[ 0.791606] loop: module loaded
[ 0.796232] megasas: 07.719.03.00-rc1
[ 0.803582] tun: Universal TUN/TAP device driver, 1.6
[ 0.809679] VFIO - User Level meta-driver version: 0.3
[ 0.815900] usbcore: registered new interface driver usb-storage
[ 0.822673] i2c_dev: i2c /dev entries driver
[ 0.828742] sdhci: Secure Digital Host Controller Interface driver
[ 0.835111] sdhci: Copyright(c) Pierre Ossman
[ 0.839815] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.846401] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.852760] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.859760] usbcore: registered new interface driver usbhid
[ 0.865464] usbhid: USB HID core driver
[ 0.870396] optee: probing for conduit method.
[ 0.875016] optee: revision 4.1 (012cdca4)
[ 0.875415] optee: dynamic shared memory is enabled
[ 0.885087] optee: initialized driver
[ 0.890846] Initializing XFRM netlink socket
[ 0.895283] NET: Registered PF_PACKET protocol family
[ 0.900547] Key type dns_resolver registered
[ 0.905416] registered taskstats version 1
[ 0.909648] Loading compiled-in X.509 certificates
[ 0.925585] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
[ 0.981102] ti-sci-clk 44043000.system-controller:clock-controller: recalc-rate failed for dev=81, clk=20, ret=-19
[ 1.011520] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.018821] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[ 1.028027] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[ 1.037428] i2c 1-003b: Fixed dependency cycle(s) with /connector
[ 1.043717] i2c 1-003b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
[ 1.051606] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.058897] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
[ 1.064961] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[ 1.074226] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 1.086536] simple-framebuffer ff700000.framebuffer: framebuffer at 0xff700000, 0x8ca000 bytes
[ 1.095404] simple-framebuffer ff700000.framebuffer: format=a8r8g8b8, mode=1920x1200x32, linelength=7680
[ 1.120909] Console: switching to colour frame buffer device 240x75
[ 1.141666] simple-framebuffer ff700000.framebuffer: fb0: simplefb registered!
[ 1.150563] ti-udma 485c0100.dma-controller: Number of rings: 82
[ 1.159177] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[ 1.170597] ti-udma 485c0000.dma-controller: Number of rings: 150
[ 1.181175] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[ 1.191736] printk: console [ttyS2] disabled
[ 1.196220] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 240, base_baud = 3000000) is a 8250
[ 1.205119] printk: console [ttyS2] enabled
[ 1.205119] printk: console [ttyS2] enabled
[ 1.213579] printk: bootconsole [ns16550a0] disabled
[ 1.213579] printk: bootconsole [ns16550a0] disabled
[ 1.225330] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[ 1.268874] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.279216] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[ 1.287330] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867
[ 1.295456] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[ 1.308461] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[ 1.314739] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[ 1.314747] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 1.315438] pps pps0: new PPS source ptp0
[ 1.332230] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[ 1.342929] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[ 1.355391] mmc0: CQHCI version 5.10
[ 1.361480] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 1.368271] pca953x 1-0022: using AI
[ 1.398351] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 1.406367] spi-nor spi0.0: n25q256ax1 (32768 Kbytes)
[ 1.411736] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
[ 1.418727] Creating 7 MTD partitions on "fc40000.spi.0":
[ 1.424198] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 1.431933] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 1.438675] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 1.445597] 0x000000680000-0x0000006c0000 : "ospi.env"
[ 1.451836] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[ 1.458682] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 1.464113] mtd: partition "ospi.rootfs" extends beyond the end of device "fc40000.spi.0" -- size truncated to 0x1800000
[ 1.476024] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[ 1.481907] mtd: partition "ospi.phypattern" is out of reach -- disabled
[ 1.497675] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 1.505996] mmc1: CQHCI version 5.10
[ 1.507421] debugfs: Directory 'pd:186' with parent 'pm_genpd' already present!
[ 1.517891] mmc2: CQHCI version 5.10
[ 1.521315] ti-sci-clk 44043000.system-controller:clock-controller: is_prepared failed for dev=81, clk=20, ret=-19
[ 1.537042] ALSA device list:
[ 1.540019] No soundcards found.
[ 1.545520] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 1.570462] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[ 1.579342] Waiting for root device PARTUUID=01cc07ea-02...
[ 1.588257] sdhci-am654 fa20000.mmc: card claims to support voltages below defined range
[ 1.608827] mmc2: new high speed SDIO card at address 0001
[ 1.611121] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 1.622275] mmcblk1: mmc1:aaaa SK32G 29.7 GiB
[ 1.629102] mmcblk1: p1 p2
[ 1.759804] EXT4-fs (mmcblk1p2): 1 orphan inode deleted
[ 1.765120] EXT4-fs (mmcblk1p2): recovery complete
[ 1.780133] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 1.789000] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.795863] devtmpfs: mounted
[ 1.800385] Freeing unused kernel memory: 1984K
[ 1.805043] Run /sbin/init as init process
[ 1.961595] systemd[1]: System time before build time, advancing clock.
[ 2.005415] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 2.037830] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.10!
[ 2.098694] systemd[1]: Hostname set to <am62xx-evm>.
[ 2.260121] systemd-sysv-generator[143]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 2.472725] systemd[1]: Configuration file /lib/systemd/system/ti-apps-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 2.503471] systemd[1]: Configuration file /lib/systemd/system/seva-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 2.554786] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 2.563748] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 2.604085] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 2.669106] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 2.746496] systemd[1]: Queued start job for default target Graphical Interface.
[ 2.812541] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 2.836719] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 2.861217] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 2.888708] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 2.913675] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password ��ts to Console Directory Watch.
[ 2.937562] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R��uests to Wall Directory Watch.
[ 2.962111] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 2.981158] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.001286] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 3.021369] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 3.100696] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 3.125572] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 3.167163] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 3.190256] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 3.217155] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 3.242680] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.266973] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 3.293375] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 3.320473] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 3.343442] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.367730] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 3.433695] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 3.469065] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 3.526013] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 3.550494] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 3.593737] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 3.618830] systemd[1]: Create List of Static Device Nodes was skipped because of a failed condition check (ConditionFileNotEmpty=/lib/modules/6.1.83-dirty/modules.devname).
[ 3.662025] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 3.686372] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 3.709823] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 3.758673] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 3.792969] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 3.817559] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[ 3.858523] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 3.889968] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 3.930241] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network ��ts from Kernel command line...
[ 3.960397] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.006143] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 4.033998] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[ 4.038926] systemd[1]: Started Start psplash boot splash screen.
[ OK ] Started Start psplash boot splash screen.
[ 4.068630] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 4.093972] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
[ OK ] Started Start psplash-syst��progress communication helper.
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
[ 4.469116] systemd-journald[157]: Received client request to flush runtime journal.
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /media/ram...
Mounting /var/volatile...
[ 4.655135] audit: type=1334 audit(1651167747.692:2): prog-id=5 op=LOAD
[ 4.666488] audit: type=1334 audit(1651167747.700:3): prog-id=6 op=LOAD
Starting Rule-based Manage��for Device Events and Files...
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on PC/SC Smart Card Daemon Activation Socket.
Starting Weston socket...
Starting D-Bus System Message Bus...
Starting Reboot and dump vmcore via kexec.[ 5.668936] random: crng init done
..
[ OK ] Listening on Docker Socket for the API.
[ OK ] Finished Load/Save Random Seed.
[ OK ] Listening on Weston socket.
[ OK ] Finished Reboot and dump vmcore via kexec.
[ OK ] Reached target Socket Units.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
Starting DEMO...
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting PulseAudio Sound System...
Starting Expand the rootfs��ll size of the boot device....
[ OK ] Started Seva Launcher Service.
[ OK ] Started strongSwan IPsec I��IKEv2 daemon using ipsec.conf.
[ 6.222297] audit: type=1334 audit(1651176038.304:4): prog-id=7 op=LOAD
[ 6.231423] audit: type=1334 audit(1651176038.312:5): prog-id=8 op=LOAD
Starting User Login Management...
[ OK ] Started TEE Supplicant.
Starting Telnet Server...
[ OK ] Started ti-apps-launcher service.
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Found device /dev/ttyS2.
[ OK ] Reached target Preparation for Network.
Starting Network Configuration...
[ OK ] Finished Telnet Server.
[ OK ] Started Telephony service.
[ OK ] Started DEMO.
[ OK ] Finished Expand the rootfs��full size of the boot device..
[ OK ] Started PulseAudio Sound System.
[ OK ] Started Network Configuration.
Starting Network Name Resolution...
[ 7.887745] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL)
[ 7.929076] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
[ 8.055122] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[ 8.077074] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[ OK ] Started User Login Management.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
[ 9.372700] audit: type=1701 audit(1651176041.452:6): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=417 comm="kmsprint" exe="/usr/bin/kmsprint" sig=6 res=1
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
[ OK ] Started Netperf Benchmark Server.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma��ent Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Created slice Slice /system/systemd-coredump.
[ 9.737436] audit: type=1334 audit(1651176041.820:7): prog-id=9 op=LOAD
[ 9.744889] audit: type=1334 audit(1651176041.824:8): prog-id=10 op=LOAD
[ OK ] Started Process Core Dump (PID 430/UID 0).
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston, a Wayland��ositor, as a system service...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ 10.131844] audit: type=1334 audit(1651176042.212:9): prog-id=11 op=LOAD
[ 10.142441] audit: type=1334 audit(1651176042.224:10): prog-id=12 op=LOAD
Starting User Database Manager...
[ OK ] Started Simple Network Man��ement Protocol (SNMP) Daemon..
[ OK ] Started User Database Manager.
[ OK ] Created slice User Slice of UID 1000.
Starting User Runtime Directory /run/user/1000...
[ OK ] Finished User Runtime Directory /run/user/1000.
Starting User Manager for UID 1000...
[ 11.605335] audit: type=1006 audit(1651176043.688:11): pid=618 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
[ 11.624248] audit: type=1300 audit(1651176043.688:11): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc9e37568 a2=4 a3=ffff98f8c020 items=0 ppid=1 pid=618 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ 11.652812] platform 2b300050.target-module: deferred probe pending
[ 11.689264] audit: type=1327 audit(1651176043.688:11): proctitle="(systemd)"
[ OK ] Started User Manager for UID 1000.
[ OK ] Started Session c1 of User weston.
[ 12.404622] audit: type=1006 audit(1651176044.484:12): pid=477 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
[ 12.424705] audit: type=1300 audit(1651176044.484:12): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc9e37568 a2=4 a3=ffff98f8c020 items=0 ppid=1 pid=477 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[ 12.468284] audit: type=1327 audit(1651176044.484:12): proctitle="(weston)"
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
Starting Weston, a Wayland��ositor, as a system service...
[ OK ] Started containerd container runtime.
[ OK ] Started Session c2 of User weston.
[ 12.840359] audit: type=1006 audit(1651176044.920:13): pid=712 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=3 res=1
[ 12.854174] audit: type=1300 audit(1651176044.920:13): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc9e37568 a2=4 a3=0 items=0 ppid=1 pid=712 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=3 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[ 12.884786] audit: type=1327 audit(1651176044.920:13): proctitle="(weston)"
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
Starting Weston, a Wayland��ositor, as a system service...
[ OK ] Started Session c3 of User weston.
[ 13.208732] audit: type=1006 audit(1651176045.288:14): pid=748 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=4 res=1
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
Starting Weston, a Wayland��ositor, as a system service...
[ OK ] Started Session c4 of User weston.
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
Starting Weston, a Wayland��ositor, as a system service...
[ OK ] Started Session c5 of User weston.
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
[FAILED] Failed to start Weston, a ��mpositor, as a system service.
See 'systemctl status weston.service' for details.
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1...
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grep
grub-common
grub-editenv
grub-efi
gzip
hidapi
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libeigen-dev
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5sensors-plugins
libqt5sensors-qmlplugins
libqt5sensors5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libqt5webchannel-plugins
libqt5webchannel-qmlplugins
libqt5webchannel5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libunistring2
m4-dev
m4
make
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquick3d-plugins
qtquick3d-qmlplugins
qtquick3d
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project am62xx-evm -
Arago 2023.10 am62xx-evm -
am62xx-evm login: [ 21.565223] kauditd_printk_skb: 13 callbacks suppressed
[ 21.565239] audit: type=1334 audit(1651176053.648:22): prog-id=14 op=UNLOAD
[ 21.578510] audit: type=1334 audit(1651176053.648:23): prog-id=13 op=UNLOAD
I hope you can offer your help.
Best Regard,
Joey