Other Parts Discussed in Thread: AM6412, AM6422, AM2434, HD3SS3220
Tool/software:
Hello,
I am designing a board using the AM6442 to support USB 3.0 with a USB Type-C connector.
For many devices, it is appropriate to set the differential impedance for SSTX and SSRX to 90Ω. However, the "High-Speed Interface Layout Guidelines" specify 95Ω for the AM6442, while some other devices specify 90Ω. Does this mean that a board designed with 90Ω impedance will not work? What is the reason for specifying 95Ω instead of 90Ω?
Additionally, the following document specifies checking the polarity of USB 3.0 signals: "AM6442, AM6422, AM6412 and AM2434 Processor Schematic Design Guidelines and Schematic Review Checklist."
Various guides and the HD3SS3220 datasheet indicate that reversing the polarity of SSTX and SSRX is acceptable. Does this mean that while many devices allow polarity reversal, the AM6442 requires correct polarity connections?
Example:
Connecting the SSRXP pin of the USB Type-C connector to the SSRXN signal and the SSRXN pin to the SSRXP signal.
Is this acceptable?

Thank you for your assistance.
Best regards,
TK0312