Part Number: PROCESSOR-SDK-J721S2
Tool/software:
J721S2 devices support two DSI outputs from Display subsystem. The first DSI output ie DSI0 is already supported in the processor SDK RTOS and this is available via DSI to DP convertor on the EVM. The second DSI output ie DSI1 is not supported in the processor SDK RTOS, as there is no device connected on the EVM for this output.
This article provides patches to enable second DSI in the Processor SDK RTOS PDK drivers.