Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
As use the default boot image from OSPI SBL image from SDK10.1, after boot up the read flash cannot work
Change the device ID to

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you tell if this is on the TI EVM or custom board?
Hi,
As use the default boot image from OSPI SBL image from SDK10.1, after boot up the read flash cannot work
Which ospi example and boot flow are you using here, and does it working with default code?
Regards,
Karthik
Hi,
default sbl_ospi_img is used, it is only for sbl. with default code
When testing with the OSPI SBL default boot image, we receive no errors. which boot flow are you using.
Log: SBL Revision: 01.00.10.01 (Dec 9 2024 - 05:16:11) TIFS ver: 10.1.6--v10.01.06 (Fiery Fox)
Regards,
Karthik
we used the SDK10.01 to build the ospi sbl default boot image, with debug profile, then start XSPI boot mode to power up. we got error.
sbl_ospi_img_mcu1_0_debug.tiimage
the EVM flash is used XSPI mode according to the sdk implementation, the read ID returns not ok, so that the handle is reset to NULL

if we direct use prebuilt image from SDK10.1 sbl_ospi_img_mcu1_0_release.tiimage , will come followed error
SBL Revision: 01.00.10.01 (Dec 9 2024 - 05:16:11)
TIFS ver: 10.1.6--v10.01.06 (Fiery Fox)
Invalid magic number in Single image header
Hi,
Invalid magic number in Single image header
For this test, are you using HS-SE devices?
Regards,
Karthik
Hi,
Change the device ID to
BOARD_FLASH_ID_S28HS512T,
Apart from these modifications, did you make any other changes?
it is normal GP device as it is EVM. but XSPI looks like some issue. we can have debug session to identify again.
It should work with TI EVM, Could you confirm that you ran this test by following the OSPI procedure below? if no please refer this.
path: /home/karthikeyansaravanan/ti/uniflash_8.7.0/ step 1: sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f /home/ti/uniflash_8.7.0/processors/FlashWriter/j784s4_evm/uart_j784s4_evm_flash_programmer_release.tiimage -i 0 step 2: sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f /home/ti/<pdk>/packages/ti/boot/sbl/binary/j784s4_evm/ospi/bin/sbl_ospi_img_mcu1_0_release.tiimage -d 3 -o 0 step 3: sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f /home/ti/<pdk>/packages/ti/drv/sciclient/soc/V6/tifs.bin -d 3 -o 0x80000 sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f /home/ti/<pdk>/packages/ti/binary/GPIO_Baremetal_LedBlink_TestApp/bin/j784s4_evm/GPIO_Baremetal_LedBlink_TestApp_mcu1_0_release.appimage -d 3 -o 0x100000 step 5: sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f /home/ti/uniflash_8.7.0/processors/FlashWriter/j784s4_evm/nor_spi_patterns.bin -d 3 -o 0x3FC0000
Regards,
Karthik
so you suggested switch to UART mode, followed commands are used
Microsoft Windows [Version 10.0.26100.2454] (c) Microsoft Corporation. All rights reserved. C:\ti\uniflash_8.7.0>dslite.bat --mode processors -c COM30 -f C:\ti\uniflash_8.7.0\processors\FlashWriter\j784s4_evm\uart_j784s4_evm_flash_programmer_release.tiimage -i 0 Executing the following command: > C:\ti\uniflash_8.7.0\processors\ProcessorSDKSerialFlash.exe -c COM30 -f C:\ti\uniflash_8.7.0\processors\FlashWriter\j784s4_evm\uart_j784s4_evm_flash_programmer_release.tiimage -i 0 For more details and examples, please refer to the UniFlash Quick Start guide. ---------------------------------------------------------------------------- ProcessorSDKSerialFlash CLI Tool Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/ Version 1.10.0.0 ---------------------------------------------------------------------------- Downloading Flash Programmer.. Transferring File of size 386145 bytes File Transfer complete! Enabling System firmware transfer!!! Header Transfer complete Transferring System Firmware.. Transferring File of size 158635 bytes File Transfer complete! C:\ti\uniflash_8.7.0>dslite.bat --mode processors -c COM30 -f W:\home\xza2abt\ti\ti-processor-sdk-rtos-j784s4-evm-10_01_00_04\pdk_j784s4_10_01_00_25\packages\ti\boot\sbl\binary\j784s4_evm\ospi\bin\sbl_ospi_img_mcu1_0_release.tiimage -d 3 -o 0 Executing the following command: > C:\ti\uniflash_8.7.0\processors\ProcessorSDKSerialFlash.exe -c COM30 -f W:\home\xza2abt\ti\ti-processor-sdk-rtos-j784s4-evm-10_01_00_04\pdk_j784s4_10_01_00_25\packages\ti\boot\sbl\binary\j784s4_evm\ospi\bin\sbl_ospi_img_mcu1_0_release.tiimage -d 3 -o 0 For more details and examples, please refer to the UniFlash Quick Start guide. ---------------------------------------------------------------------------- ProcessorSDKSerialFlash CLI Tool Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/ Version 1.10.0.0 ---------------------------------------------------------------------------- Transferring the Image to Flash Programmer.. Transferring Header Information.. Header Transfer Complete! Flashing Image of size 353455 bytes Flash Programming Success! C:\ti\uniflash_8.7.0>dslite.bat --mode processors -c COM30 -f W:\home\xza2abt\ti\ti-processor-sdk-rtos-j784s4-evm-10_01_00_04\pdk_j784s4_10_01_00_25\packages\ti\drv\sciclient\soc\V6\tifs.bin -d 3 -o 0x80000 Executing the following command: > C:\ti\uniflash_8.7.0\processors\ProcessorSDKSerialFlash.exe -c COM30 -f W:\home\xza2abt\ti\ti-processor-sdk-rtos-j784s4-evm-10_01_00_04\pdk_j784s4_10_01_00_25\packages\ti\drv\sciclient\soc\V6\tifs.bin -d 3 -o 0x80000 For more details and examples, please refer to the UniFlash Quick Start guide. ---------------------------------------------------------------------------- ProcessorSDKSerialFlash CLI Tool Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/ Version 1.10.0.0 ---------------------------------------------------------------------------- Transferring the Image to Flash Programmer.. Transferring Header Information.. Header Transfer Complete! Flashing Image of size 158666 bytes Flash Programming Success! C:\ti\uniflash_8.7.0>dslite.bat --mode processors -c COM30 -f W:\home\xza2abt\ti\ti-processor-sdk-rtos-j784s4-evm-10_01_00_04\pdk_j784s4_10_01_00_25\packages\ti\binary\GPIO_Baremetal_LedBlink_TestApp\bin\j784s4_evm\GPIO_Baremetal_LedBlink_TestApp_mcu1_0_release.appimage -d 3 -o 0x100000 Executing the following command: > C:\ti\uniflash_8.7.0\processors\ProcessorSDKSerialFlash.exe -c COM30 -f W:\home\xza2abt\ti\ti-processor-sdk-rtos-j784s4-evm-10_01_00_04\pdk_j784s4_10_01_00_25\packages\ti\binary\GPIO_Baremetal_LedBlink_TestApp\bin\j784s4_evm\GPIO_Baremetal_LedBlink_TestApp_mcu1_0_release.appimage -d 3 -o 0x100000 For more details and examples, please refer to the UniFlash Quick Start guide. ---------------------------------------------------------------------------- ProcessorSDKSerialFlash CLI Tool Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/ Version 1.10.0.0 ---------------------------------------------------------------------------- Transferring the Image to Flash Programmer.. Transferring Header Information.. Header Transfer Complete! Flashing Image of size 152436 bytes Flash Programming Success! C:\ti\uniflash_8.7.0>dslite.bat --mode processors -c COM30 -f C:\ti\uniflash_8.7.0\processors\FlashWriter\j721e_evm\nor_spi_patterns.bin -d 3 -o 0x03FC0000 Executing the following command: > C:\ti\uniflash_8.7.0\processors\ProcessorSDKSerialFlash.exe -c COM30 -f C:\ti\uniflash_8.7.0\processors\FlashWriter\j721e_evm\nor_spi_patterns.bin -d 3 -o 0x03FC0000 For more details and examples, please refer to the UniFlash Quick Start guide. ---------------------------------------------------------------------------- ProcessorSDKSerialFlash CLI Tool Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/ Version 1.10.0.0 ---------------------------------------------------------------------------- Transferring the Image to Flash Programmer.. Transferring Header Information.. Header Transfer Complete! Flashing Image of size 128 bytes Flash Programming Success! C:\ti\uniflash_8.7.0>
after that come back to XSPI mode
Output of MCU_UART is only with

Hi,
Output of MCU_UART is only with
Board flashopen seems to have been successful on your evm. Instead of using GPIO_Baremetal_LedBlink_TestApp, could you please use the UART_TestApp_freertos driver example?
Regards,
Karthik
Hi,
i just tried with debug image of GPIO_Baremetal_LedBlink_TestApp, it prints out the test passed massage. I think the 3rd party debug flashing script has issue. Thnaks.
but still some question : uniflash version must be 8.7.0? 9.0.0 is not suitable? How to erase the OSPI , have you some general commands for usage?
Hi,
uniflash version must be 8.7.0? 9.0.0 is not suitable? How to erase the OSPI , have you some general commands for usage?
I am not sure about this .
How to erase the OSPI
Could you please refer this https://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/index_board.html#erasing-the-flash-device link let us know if this helps.
Regards,
Karthik