Other Parts Discussed in Thread: DRA829, DRA821
Tool/software:
Hi,
We have seen leakage problems for VSYS_MCUIO_3V3 (U22) and VSYS_IO_3V3 (U6). Both rails are supplied by VSYS_3V3 and each rail is controlled by a load switch (see attached schematic).
During disabling PMIC_EN we can see that the Voltage on VSYS_IO_3V3 only goes down to ~1,76V and the VSYS_MCUIO_3V3 goes down to ~1,5V (see attached pictures 1&2).
We have already verified that the two load switches U6 and U22 are fully disabled via the control signals (low state confirmed).
For the VSYS_MCUIO_3V3 we have found that when VOUT_LDOVINT (PMICA and PMICB) are disable (LP_STANDBY_SEL=1) the leakage goes down to ~0.8V.
We have removed all peripherals connected to the VSYS_IO_3V3 and we could only see that the voltage increased when different loads (peripherals) were disconnected from the rail.
Our conclusion is now that the leakage source comes from the MPU (DRA829VMT0CALFRQ1) only.
The power up and down sequence are affected by this leakage and will not fulfil the power down/ up timing diagrams of the DRA829 datasheet.
We have not seen any negative impact affecting the performance from our testing but would like to get this confirmed by you because the power up and down sequence are not fulfilled
according to the DRA829 datasheet.
Could this affect the performance in any way if the power rails (VSYS_MCUIO_3V3 and VSYS_IO_3V3) doesn't turn off completely?
Thanks for your support!
Best regards
/Mathias Sixtander

Picture1: Leakage on VSYS_MCUIO_3V3

Picture2: Leakage on VSYS_IO_3V3