Tool/software:
Hi,
I am currently working on implementing a Driver Monitoring System using the TI AM62A Starter Kit.
The use case is to build a object detection model to detect and alert the driver in case of following conditions.
1. Eye drowsiness detection
2. Yawning detection
3. Distracted detection
4. Phone call detection
5. Smoking detection
6. No driver detection
7. Head phone detection to the extent possible
8. Camera covered