Tool/software:
Hi,
I have followed the below link and found that my device was "HSFS".
Link: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_01_00_08/exports/docs/linux/Foundational_Components_Migration_Guide.html
Next, I have downloaded the tisdk-default-image-am62pxx-evm-10.01.10.04.rootfs.wic.xz image and followed the procedures in the below link for flashing the device.
Link: https://dev.ti.com/tirex/content/tirex-product-tree/processors-devtools_1_00_02/am62px_skevm_quick_start_guide.html
After Flashing, I could not see any logs in the UART and also there is no output in the HDMI.
Note:
1. Android is flashed in emmc and Linux is flashed in SD card. When we change the switch to emmc boot mode, Android is booting properly. After changing the switch to Linux mode, There is no logs in the serial console. The switches are properly configured as in the link.
2. From Android OS, I verified the detection of SD card.
3. Checked the partitions in the SD card, There are two partitions in it.
Kindly help to resolve the issue. Thanks in Advance!!