Tool/software:
I am working with the TMS320C641T DSP and an FPGA in my project, and I would like to understand the clock synchronization requirements when these two devices communicate with each other.
Could you please clarify which clock signal is used to synchronize the communication between the TMS320C641T DSP and the FPGA? Is the CLKIN signal from the DSP used for synchronization, or is there another clock source recommended for this type of communication?
Additionally, if there are any specific considerations for timing, clock distribution, or configuration to ensure reliable communication between the DSP and FPGA, I would appreciate any references to relevant sections of the datasheet, application notes, or guidelines.