Other Parts Discussed in Thread: TM4C1294NCPDT, EK-TM4C1294XL
Tool/software:
Hello,
I have just installed the lastest CCS 20.1.0. However, I cannot create a single project for the TM4C1294XL evaluation board or even an empty project for a custom board. I keep getting an error message for the evaluation board about compiler not available.
If I try to create a new project and enter the device part number in for TM4C1294NCPDT, there is on option at all for creating a project.
What is going on with this newest version of CCS? I need to create projects around this microcontroller family and I find that nothing is working in the new Theia based versions.
How can a get the example projects to work or get a standard empty project that works with the TivaWare SDK?
I have tried the "Import" as well and it does not allow compiling of the projects because of the following error.