This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: RPMSG Delay

Part Number: TDA4VM


Tool/software:

Hello,Export:

Test the communication delay time of rpmsg between A72 and MCU1-0 :


Scenario 1: Simple PING PONG sending and receiving between A72 and MCU1-0. The delay of sending and receiving is about 50ms in the test on A72.


Scenario 2: There are two tasks on MCU1-0. The two tasks send data to A72 at a period of 100ms, and then A72 and MCU1-0 perform a PING PONG sending and receiving delay test. The maximum delay is more than 400 ms and the minimum delay is 2ms.


What is the normal rpmsg communication delay time? Is there any problem with the above data?