Other Parts Discussed in Thread: AM62L
Tool/software:
Dear TI Support,
An issue has been observed on the AM62L EVM while conducting an Ethernet dependency test. When modifying the k3-am62lx-evm.dts to disable one of the two Ethernet ports, the remaining enabled port fails to obtain an IP address via DHCP. This behavior is consistent in both directions—disabling either port causes the other to stop receiving an IP address. With both ports enabled in the default device tree, both interfaces function as expected.
Attached is the dts changes done. While doing so MAC address is getting assigned by the command "ifconfig eth0 hw ether...." but IP is not assigning.
Is there any dependancy between two ethernet ports.How to test since i have only one ethernet port in my custmised board. Could you please guide me through this issue.
Regards,
Dheeraj K