Other Parts Discussed in Thread: DM388,
Tool/software:
Hi team,
1. My customer will replace the IC (DM388AAAR11) used in the internal board of the equipment. They are considering whether the DM385AAAR11F can be used. * They are aware that each IC has already been discontinued.
Do we have any new product replacement for DM388 or DM385 ?
2. Regarding the firmware that is written to the DM388 currently being used in the current circuit pack,
If customer is not using the noise filter or face detect features which is the difference between DM388 and DM385,
is it possible to confirm whether the current firmware can work on the DM385 or not ?
Best regards,
Kenley