HW:DM8168
I has test 1080I60 capture in EZSDK5.03.0.09,it works normally.
but when the same code is moved to EZSDK5.03.1.15,the 1080I60 capture will block after capture a few frames.
why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HW:DM8168
I has test 1080I60 capture in EZSDK5.03.0.09,it works normally.
but when the same code is moved to EZSDK5.03.1.15,the 1080I60 capture will block after capture a few frames.
why?
Hi,
FieldMerged support for Interlaced input has been added in OMX.VFCC component.
We have tested interlaced capture in 5.03.01.15 and it seems to be working fine. Can you share the firmware trace as per the instructions given at http://processors.wiki.ti.com/index.php/OMX_Viewing_Media_Controller_Traces?
Regards,
Anirban