Sorry newbie alert - well to ti anyway.
I have gotten the job of integrating 2 branches of code that branched some years back.
On the one branch I have a couple of ccs v3.1 (bios 4.9 cgt 5.1.9) projects (one 6412 and one 6415 based) which are the main line products, for reasons I think I am just discovering my predecessor did not upgrade for years.
The other, externally sourced, branch I have to pull in without damaging the important branch, this has some newly developed code for a 6433 that uses ccs v5 (at least briefly to set stuff up, now it is just a gmake file) with bios 6.30.02.42 and cgt 7.3.1.
All the usual politics apply so I cannot get the external branch redone in an earlier version, not sure the newer DSP is even supported on the old tools and I must merge the products which nominally are a common code base.
My plan is to upgrade the main programs to the latest version then do the massive merge by hand.
I hit a hitch right away, the ccs v5 import wizard only understands ccs v3.3 files so I went via v3.3 to get to v5. The end result was it did compile with a little help but does not run at all.
I went back to do it step by step, using v3.3 ide with the bios and cgt from the v3.1 build, then stepping up the compiler and the tools individually.
Step 1.ccs v3.3 with old cgt and bios - no compile, ccs wants to work with tconf rather than cbd bios config files.
Step 2 ccs v3.3 with old cgt and bios 5.31.02 - builds but fails to run.
I am hoping someone here remembers the v3.1 to v3.3 pain and can advise me. I suspect the CDB to Tconf conversion is the root of my problems.
And in general am I wasting my time with the import wizards should I start with hello world and try to recreate the projects from scratch
Thanks in hope
Chris
ps I expect the question, when I say it did not run, how did it crash - don't know, I have a parallel port emulator and no PCs handy with a parallel port, and even if I buy a USB emulator the revision of the boards I have to test with has never been used with an emulator and no one remembers the jtag mods required...