Part Number: AM6442
Tool/software:
Hi Support Team,
I apologize for regarding a thread that has been ongoing for some time,
but I have additional questions regarding the following site.
The customer is using Single Write, Non-Multiplexed, so only the first transfer will be performed.
In the case of Single Write, Non-Multiplexed, referring to
Figure 6-43. GPMC and Multiplexed NOR Flash — Synchronous Burst Write
in the datasheet, please let me know what the value of “F15” would be.
Please confirm the appropriate value below.

To clarify, the question in the image is as follows.
Q1. F15 is specified for Transition. Here, the minimum is 17.7 ns, but
the maximum is 22.7 ns, so it cannot be captured even in the next clock.
If it is specified for Setup, I think 17.7 ns is reasonable, but is that correct?
Q2. F15 is specified for Transition. Here, if it is specified for Hold,
I think 22.7 ns is reasonable for the maximum, but is that correct?
.
I would also like to confirm the timing diagram and specification values for Single Write and Multiplexed cases.
Best Regards,
Kanae