Tool/software:
We use PCIe (SERDES0 and SERDES2) of DRA829J-Q1 with Gen1, Jacinto is root complex.
AC coupling capacitor is 100nF, placed close to the transmitter.
Measurement shows a common mode voltage of 0V at the Jacinto receiver input.
Despite there is no negative reference connected to Jacinto pins, our expectation is that Jacinto is capable to evaluate the full differential voltage even if one SERDES RX input pin is at negative potential.
Or is the common mode voltage of the SERDES Receiver adjustable via register setting?
Regards, Peter