Other Parts Discussed in Thread: AM67, LMK3H0102, AM62P
Hi TI Experts,
Can you provide a List of collaterals and E2E that can be referred when starting a custom board hardware design.
Hi Board designers,
AM67A, AM67 processor family is available on TI.com and is in preview.
The below links are a quick reference to the collaterals that can be referred when starting a custom design.
Device Selection and features
Product Pages
https://www.ti.com/product/AM67
https://www.ti.com/product/AM67A
Data Sheet
AM67x Processors datasheet
https://www.ti.com/lit/pdf/sprspa3
Datasheet
AM62Dx Sitara Processors datasheet
https://www.ti.com/lit/pdf/sprspb5
Silicon Errata
J722S TDA4VEN TDA4AEN AM67 Processor Silicon Revision 1.0 Errata (Rev. A)
https://www.ti.com/lit/pdf/sprz575
Technical Reference Manual (TRM)
J722S TDA4VEN TDA4AEN AM67 Processor Silicon Revision 1.0 Technical Reference Manual (Rev. B)
https://www.ti.com/lit/zip/sprujb3
Custom Board design:
Schematic Design and Review Checklist
Jacinto7 AM6x/TDA4x/DRA8x Schematic Checklist (Rev. B)
https://www.ti.com/lit/pdf/sprad91
Power Consumption
AM67A AM67 Power Estimation Tool
J722S/TDA4VEN/TDA4AEN/AM67 Power Estimation Tool User’s Guide (Rev. A)
https://www.ti.com/lit/zip/sprujd0
Maximum Current Ratings
Evaluation - EVM
https://www.ti.com/tool/J722SXH01EVM
https://www.ti.com/tool/BEAGLEY-AI
Schematics (Reference) for RMII interface
Note: We did functionally validate the common clock configuration. No other clocking options were tested.
Ethernet PHY daughter card
https://www.ti.com/tool/DP83867-EVM-AM
https://www.ti.com/tool/DP83826-EVM-AM2
https://www.ti.com/tool/TIDA-00928
Jacinto 7 LPDDR4 Board Design and Layout Guidelines (Rev. F)
DDR Board Design and Layout Guidelines
https://www.ti.com/lit/pdf/spracn9
TÜV SÜD Certificate for Functional Safety Software Development Process (Rev. D)
https://www.ti.com/lit/pdf/szzq188
Regards,
Sreenivasa
Hi Board designers,
FAQs for reference
e2e.ti.com/.../am67a-general-question-of-am67a
e2e.ti.com/.../am67a-die-registers-of-the-am67a
e2e.ti.com/.../am67a-seeking-guidance-for-development-am67a
e2e.ti.com/.../am67a-how-to-increase-the-clock-frequency-of-r5f-mcu-core-in-am67a
e2e.ti.com/.../am67a-purpose-of-the-reset-lines-and-reset-outputs
e2e.ti.com/.../am67a-importance-of-ddrss-register-configuration-tool-for-bring-up-custom-board
e2e.ti.com/.../am62a7-q1-c7x-mma-versions-between-am62a-and-tda4ven
e2e.ti.com/.../am67a-pdn-impedance-requirements
e2e.ti.com/.../am67a-soc-package-delay
e2e.ti.com/.../5812246
e2e.ti.com/.../am67a-layout-questions
e2e.ti.com/.../am67a-minimum-decapling-capacitor-for-vdd_core
e2e.ti.com/.../am67a-am67a-evb-grounds-question
e2e.ti.com/.../am67a-external-reference-clock-requirement-for-serdes-function
e2e.ti.com/.../am67a-trace-requirement-for-pcie-reference-clock
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1565204/j722sxh01evm-question-for-extenal-clock-source-of-pcie
e2e.ti.com/.../am67a-pcie-reference-clock
1 - yes AM67A has several errata items related to PCIe and specifically clocks. I can't say is necessary to use external clock - that is dependent on how you are using PCIe and if the errata items will impact you. But certainly some of the work-arounds for the issue(s) involve using an external refclk.
2 - No in-line capacitor is required. LMK3H0102 can be connected directly to AM67 and PCIe connector/peripheral.
e2e.ti.com/.../am67a-can-the-pcie-subsystem-be-used-with-serdes0-or-only-with-serdes1
Yes, I see that figure 12-121 mention wrongly that the PCIe is supported on SERDES0. It is a mistake; only SERDES1 supports PCIe on AM67.
e2e.ti.com/.../am67a-how-to-generate-pcie-reset
e2e.ti.com/.../am67a-implementing-usb_id-on-a-custom-design
e2e.ti.com/.../am67a-partial-io-peripherals
e2e.ti.com/.../am67a-wkup_uart-mcu_uart-usage
e2e.ti.com/.../faq-tda4vm-dra829v-j721e-how-to-enable-ehrpwm-on-j7-evm-using-linux
e2e.ti.com/.../am67a-is-external-rtc-needed
e2e.ti.com/.../am67a-if-not-using-can-jtag-pins-be-left-as-unterminated-nc
e2e.ti.com/.../am67a-what-is-the-value-of-the-pin-pull-up-and-pull-down-resistors
e2e.ti.com/.../am67a-can-t-the-oldi-pins-be-configured-as-gpio
e2e.ti.com/.../am67a-design-guide-xspi-boot-mode-and-lbclk
I got a response from the ROM expert and he confirmed that OSPI0_LBCLK is not configured or used by ROM, so that particular pin can be used for some other config.
Internal reference clock with Taps that the Boot ROM supports with QSPI, OSPI and XSPI(With PHY disabled) boot modes.
For QSPI and OSPI boot, OSPI0_CLK frequency is 50MHz (Where internal reference clock is 200MHz). ROM has a way of learning the optimal tap settings, which is configured during boot.
While for xSPI boot without PHY, OSPI0_CLK frequency is 25MHz.
e2e.ti.com/.../am67a-can-gb-ethernet-be-operated-on-the-r5f-core
The SDK for AM67A supports the controlling the CPSW ethernet switch from a native Linux driver running on A53.
software-dl.ti.com/jacinto7/esd/processor-sdk-linux-am67a/11_00_00/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/Network/CPSW-Ethernet.html
While I did not find specific documentation for AM67A for an example of CPSW Ethernet on R5F core, on AM62P (which also has an R5F core), there are examples of setting up CPSW Ethernet to run on R5F via the MCU+SDK. For example: software-dl.ti.com/.../EXAMPLES_ENET_LWIP_CPSW.html
To my knowledge there is no plan for an MCU+SDK for AM67 so finding examples of Ethernet on R5F directly may not be difficult.
e2e.ti.com/.../am67a-pinctrl-of-gpio-pu-pd-seems-overwritten-when-requesting-the-line-via-gpiod
e2e.ti.com/.../am67a-how-to-connect-the-switch-chip
e2e.ti.com/.../am67a-internal-rgmii-delay
e2e.ti.com/.../am67a-video-audio-requirements-check
e2e.ti.com/.../am67a-are-there-any-differences-between-the-4-csi-camera-ports
www.ti.com/.../spradh2a.pdf
e2e.ti.com/.../faq-am67a-enabling-csi2-sensors-via-fusion-board-on-am6x
e2e.ti.com/.../tda4ven-q1-multi-camera-input-using-mipi-virtual-channel
e2e.ti.com/.../am67a-does-ti-soc-have-plans-to-support-4x8mb-or-1x12mb-camera-sensor-and-usb-3-0
e2e.ti.com/.../am67a-isp-without-lpddr4
Regards,
Sreenivasa
Hi Board Designers,
E2E related to PMIC
J722S/AM67x/TDA4VEN/TDA4AEN Processor Automotive Power Designs using TPS6522312-Q1 PMIC
www.ti.com/.../sprt775
Regards,
Sreenivasa
Hi Board Designers,
E2E related to LPDDR4
e2e.ti.com/.../am67a-lpddr4-routing-topology
e2e.ti.com/.../am67a-lpddr4-layout-recommendatio
Regards,
Sreenivasa
Hi Board Designers,
FYI
AM67A: Request for Guidance on C7x Core Software Development (AM67A)
Please note that TI doesn`t support Beagle Y AI platform on TI E2E forums. Currently AM67A product is designed for C7x DSP to be used as DL compute accelerators. There is currently no roadmap available to enable C7x to be used as a DSP compute accelerator rather than DL accelerator. I am looping in relevant expert from productline who can indicate if there is future plan to support the platform and offer C7x DSP development option on this platform or if they can provide information for partners who may be able to support you outside of the TI standard offering to port/develop code on this platform.
Regards,
Sreenivasa
Hi Board Designers,
Inputs related to IBIS-AMI model availability
(+) AM67A: IBIS-AMI model request - Processors forum - Processors - TI E2E support forums
AM67A: IBIS-AMI model request
I understand that the IBIS-AMI models are shared under NDA.
Please reach out to the filed team you are working to take this forward.
Regards,
Sreenivasa