This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: Error message when JTAG debugging AM4378

Part Number: AM4378

 
 
 
While debugging an AM4378 using CCS, the following error was output from CCS on one of several dozen boards.
 
CortexA9: Error connecting to the target: (Error -1324 @ 0x3A654) Device failed to enter debug/halt mode (cannot determine cause). Power-cycle the board. If the error persists, confirm configuration and/or try more reliable JTAG settings (e.g., lower TCLK). (Emulation package 7.0.48.0)
 
Changing the TCLK frequency to 100 kHz in the CCS settings did not resolve the issue.
I am using Code Composer Studio 7.3.0.
  • Hello,

    Can you try testing your JTAG connection as shown in the video below?

    https://dev.ti.com/tirex/explore/node?node=A__AMCrhRy9n80ZsUrBFVdo1Q__ccs_devtools__FUz-xrs__LATEST

    Copy and paste the test results to this thread.

    Thanks

    ki

  • Thank you for your reply,Ki

    I tried Test Connection as shown in the video.

    I will post the results.

    [Start: Blackhawk XDS560v2-USB System Trace Emulator_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\108649\AppData\Local\TEXASI~1\CCS\
    ti\0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'bh560v2u.out'.
    Loaded FPGA Image: C:\ti\ccsv7\ccs_base\common\uscif\dtc_top.jbc
    The library build date was 'Jul 21 2017'.
    The library build time was '18:30:42'.
    The library package version is '7.0.48.0'.
    The library component version is '35.35.0.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '6' (0x00000006).
    The controller has an insertion length of '0' (0x00000000).
    The cable+pod has a version number of '8' (0x00000008).
    The cable+pod has a capability number of '7423' (0x00001cff).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.

    -----[Print the reset-command hardware log-file]-----------------------------

    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the Nano-TBC VHDL.
    The link is a 560-class second-generation-560 cable.
    The software is configured for Nano-TBC VHDL features.
    The controller will be software reset via its registers.
    The controller has a logic ONE on its EMU[0] input pin.
    The controller has a logic ONE on its EMU[1] input pin.
    The controller will use falling-edge timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '2' (0x0002).
    The utility logic has not previously detected a power-loss.
    The utility logic is not currently detecting a power-loss.
    Loaded FPGA Image: C:\ti\ccsv7\ccs_base\common\uscif\dtc_top.jbc

    -----[The log-file for the JTAG TCLK output generated from the PLL]----------

    Test Size Coord MHz Flag Result Description
    ~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~
    1 none - 01 00 500.0kHz - similar isit internal clock
    2 none - 01 09 570.3kHz - similar isit internal clock
    3 64 - 01 00 500.0kHz O good value measure path length
    4 16 - 01 00 500.0kHz O good value auto step initial
    5 16 - 01 0D 601.6kHz O good value auto step delta
    6 16 - 01 1C 718.8kHz O good value auto step delta
    7 16 - 01 2E 859.4kHz O good value auto step delta
    8 16 + 00 02 1.031MHz O good value auto step delta
    9 16 + 00 0F 1.234MHz O good value auto step delta
    10 16 + 00 1F 1.484MHz O good value auto step delta
    11 16 + 00 32 1.781MHz O good value auto step delta
    12 16 + 01 04 2.125MHz O good value auto step delta
    13 16 + 01 11 2.531MHz O good value auto step delta
    14 16 + 01 21 3.031MHz O good value auto step delta
    15 16 + 01 34 3.625MHz O good value auto step delta
    16 16 + 02 05 4.313MHz O good value auto step delta
    17 16 + 02 13 5.188MHz O good value auto step delta
    18 16 + 02 23 6.188MHz O good value auto step delta
    19 16 + 02 37 7.438MHz O good value auto step delta
    20 16 + 03 07 8.875MHz O good value auto step delta
    21 16 + 03 15 10.63MHz O good value auto step delta
    22 16 + 03 1E 11.75MHz {O} good value auto step delta
    23 64 + 02 3E 7.875MHz O good value auto power initial
    24 64 + 03 0E 9.750MHz O good value auto power delta
    25 64 + 03 16 10.75MHz O good value auto power delta
    26 64 + 03 1A 11.25MHz O good value auto power delta
    27 64 + 03 1C 11.50MHz O good value auto power delta
    28 64 + 03 1D 11.63MHz O good value auto power delta
    29 64 + 03 1D 11.63MHz O good value auto power delta
    30 64 + 03 13 10.38MHz {O} good value auto margin initial

    The first internal/external clock test resuts are:
    The expect frequency was 500000Hz.
    The actual frequency was 499110Hz.
    The delta frequency was 890Hz.

    The second internal/external clock test resuts are:
    The expect frequency was 570312Hz.
    The actual frequency was 569976Hz.
    The delta frequency was 336Hz.

    In the scan-path tests:
    The test length was 2048 bits.
    The JTAG IR length was 6 bits.
    The JTAG DR length was 1 bits.

    The IR/DR scan-path tests used 30 frequencies.
    The IR/DR scan-path tests used 500.0kHz as the initial frequency.
    The IR/DR scan-path tests used 11.75MHz as the highest frequency.
    The IR/DR scan-path tests used 10.38MHz as the final frequency.

    -----[Measure the source and frequency of the final JTAG TCLKR input]--------

    The frequency of the JTAG TCLKR input is measured as 10.37MHz.

    The frequency of the JTAG TCLKR input and TCLKO output signals are similar.
    The target system likely uses the TCLKO output from the emulator PLL.

    -----[Perform the standard path-length test on the JTAG IR and DR]-----------

    This path-length test uses blocks of 64 32-bit words.

    The test for the JTAG IR instruction path-length succeeded.
    The JTAG IR instruction path-length is 6 bits.

    The test for the JTAG DR bypass path-length succeeded.
    The JTAG DR bypass path-length is 1 bits.

    -----[Perform the Integrity scan-test on the JTAG IR]------------------------

    This test will use blocks of 64 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG IR Integrity scan-test has succeeded.

    -----[Perform the Integrity scan-test on the JTAG DR]------------------------

    This test will use blocks of 64 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG DR Integrity scan-test has succeeded.

    [End: Blackhawk XDS560v2-USB System Trace Emulator_0]

  • Thank you. The low level JTAG connection between the CCS debugger and the device appears good. Based on the error message in your first post, the issue looks specific to some device initialization/configuration issue. Basically the device is not in the proper state for debug access. I will bring this thread to the attention of the device experts for further suggestions.

  • Hi,

    Are you running RTOS SDK on the AM43? And does this error show up when debugging your RTOS application?

    Regards

    Karan

  • Thank you for your reply,Karan Saxena

    >Are you running RTOS SDK on the AM43?

    Yes, I use the RTOS SDK.

    >does this error show up when debugging your RTOS application?

    Even if you remove the RTOS application, an error will be displayed when starting the debugger.

  • Hello,

    We no longer support baremetal or TI-RTOS based SW development on AM437x. Please refer to this announcement and find resources there:

     Notice regarding Processor SDK TI-RTOS for AM335x, AM437x, OMAP-L13x, C674x, K2G, AMIC110, AMIC120 devices 

    Regards,

    Jianzhong