This article provides SW interface to enable/disable and to configure watchdog timer for VHWA modules
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This article provides SW interface to enable/disable and to configure watchdog timer for VHWA modules
Please find attached patch on top of PSDK RTOS 11.1 release. This patch provides interface to control WDG timer for VHWA modules.
- This patch disables WDG timer by default for all VHWA modules.
- It also adds a new control command IOCTL_VHWA_M2M_{VHWA Module name}_CONFIG_WDTIMER to control parameters of the WDG timer.
- This control command can be called after call SET_PARAMS ioctl.
- Please apply this patch on top of ti-processor-sdk-rtos-j721s2-evm-11_01_00_04\pdk_j721s2_11_01_00_17 folder and rebuild the PDK/SDK.
Regards,
Brijesh