This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: VDD_Core Changing Voltage using TPS65219

Part Number: AM625
Other Parts Discussed in Thread: SK-AM62B-P1,

Hello,

I confirmed with the PMIC team that once powered up, the PMIC can be commanded through I2C to change the voltage of any of the Bucks (1-3). For the case in which my customer wants to run some temperature characterizations on the AM625 with VDD_CORE = 0.75V while using the SK-AM62B-P1 EVM, I was thinking they could simply throw an I2C command from the processor to the PMIC and tell the PMIC to set Buck1 to 0.75V. Is the processor capable of this transition from VDD_CORE of 0.85V to 0.75V?

Best,

Jason Maxwell