This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: IMX623 camera bring up based on Des MAX96712 with Ser MAX96717

Part Number: TDA4VL-Q1

 IMX623 camera bring up based on Des MAX96712 with Ser MAX96717 
I am facing the same timeout error as below ticket 
Can you please suggest the solution whcih was discussed in thsi ticket?
TDA4VM: TDA4VM new camera bring up based on Des MAX96712 - Processors forum - Processors - TI E2E support forums 

  • Hi ,

    Are you seeing this error?

    [MCU2_0] 37.364024 s: VX_ZONE_WARNING:[tivxCaptureSetTimeout:760] CAPTURE: WARNING: Error frame not provided using tivxCaptureRegisterErrorFrame, defaulting to waiting forever !!!

    The solution was changing the I2C register settings for the deserializer.

    The customer set:

    • register 0xf0 to value 0x61 
    • register oxf1 set to value 0x76

    There is likely an issue with your deserializer settings.

    Best,
    Jared