This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VPE-Q1: Pin muxing issues

Part Number: TDA4VPE-Q1

we are designing SOM and Baseboard for TDA4APE6T5AANDRQ1 

below is the screenshot of Pin mux tool for PCIe:
   


below is the screenshot of Pin mux tool for SGMII:
   
below is the screenshot of Pin mux tool for USB:
   


Below are the queries:
1. for PCIe1 upto 2L can be configured, 4 lanes not possible(showing error), can we split PCIe1 into
two individual lanes (1 lane forNvme ssd and another lane for PCIe to dual sata bridge)?

note: usb 3.0 all signals are muxed.

2. In SGMII5, TX lines are not showing even if pin mux tool is started fresh. How to find tx lines.

PCIe Devices we have are as below:
1. M.2 nvme ssd with PCIe gen 3 x1

2. PCIe to dual sata with PCIe gen 2 x 1