Part Number: AM2754-Q1
Other Parts Discussed in Thread: MATHLIB
Hi,
Is a C++ compiler required to use the C7x Math Library(Mathlib)?
Thanks and Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
You need TI CGT C7000 compiler fro the library: https://www.ti.com/tool/C7000-CGT .
Thanks,
Shreyansh
Hi IChung,
I am sorry, I don't fully understand the issue. Can you please share the error you are getting and compiler flags you are using? Are you building for Host Emulation/PC or EVM?
Thanks,
Shreyansh
In the included header file MATHLIB_type.h, the following structure definition appears at line 153:
As far as I know, providing default initializers for structure members is not allowed in C, and is only valid in C++ (C++11 and later).
Because of this, a compilation error occurs when building with a C compiler.
Therefore, I would like to ask:
Is the Mathlib library intended to be compiled with a C++ compiler rather than a C compiler?
Hi IChung,
typedef struct {
bool callCheckParams = false;
bool callInit = true;
__SE_TEMPLATE_v1 se0Params;
__SE_TEMPLATE_v1 se1Params;
__SA_TEMPLATE_v1 sa0Params;
size_t blockSize = 0;
} MATHLIB_SESA1DSequential_t;As far as I know, providing default initializers for structure members is not allowed in C,
That's correct and is one of the reasons why the library is written in C++. However, as long as you are compiling the library for a target, all you need is the TI CGT C7000 compiler, it can compile both C and C++ files.
Refer to the compiler doc: www.ti.com/.../spruig8g.pdf
Thanks,
Shreyansh