Sorry for the novice question. I've got a BeagleBoard that has a fairly large SD card in it and I was wondering if I could actually run Eclipse on the BeagleBoard itself and compile Gnu C application stuff on the actual BeagleBoard rather than cross-compiling under Debian on an Intel machine. Can someone kindly point me to a load of the Eclipse IDE if there is such a thing? Thanks!