This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VPE-Q1: Contact EVM circuit diagram

Part Number: TDA4VPE-Q1

Hello
We are developing using TDA4VPE-Q1.

TI homepage is making a circuit with EVM BOARD data (spac001a.ZIP) among TDA4VPE-Q1 related data.
www.ti.com/.../J742S2XH01EVM

1. There is a difference in the circuit diagram. In PROC184E2_SCH.DSN and PROC184E2(002)_SCH.pdf, there is a difference in the parts that are mis-treated as DNI. Based on which circuit diagram should I develop it?

2. The PROC184E2(002)_BOM.xlsx BOM file is PROC184E2_SCH.DSN and PROC184E2(002)_SCH.pdf, which file is the BOM?

Thank you.

  • Regarding the schematic - version E2 is the latest.  The design source file (Cadence OrCad) is PROC184E2_SCH.DSN.  The PDF version is PROC184E2(001)_SCH.pdf.  Note the DSN file includes variants, different assembly options.  Variant 001 is the correct assembly version.

    Regarding the bill of materials - again 001 is the correct variant.  Thus the correct file is PROC184E2(001)_BOM.xlsx