This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VPE-Q1: unable to MUX PCIe - CLKREQn pin when SDcard enabled

Part Number: TDA4VPE-Q1

SOC used here: TDA4APE6-Q1 

We want to use both SDcard(MMC_1) and PCIe1 port in the Board.
 
MMC_1 Cd pin interferes with PCIe1 - CLKREQn
 
 
 
I see that PCIe1 - CLKREQn  is used for transitioning to and from low power states, Here it is done without Wake signal pin. 
 
 
My question is:
 
Once the SOC bootsup through SDcard with CD pin, Can I Remux CD pin to CLKREQn?
 
If I dont want to transition to PCIe Low power states, can I use this pin for SDcard - CD pin and leave CLKREQn  optional?