This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to install DM6467T VDCE dirver in my system?



Hi,

I am using a DM6467T application platform developed by the third party. I think the linux is a little different from DM6467EVM. The linix kernal name is "Linux/armv5tejl 2.6.33-lusim-1.1.1" which I can see when logging in. 

There is no VDCE driver in the linux and no device named "/dev/DavinciHD_vdce".

How can I install the VDCE driver?

 Or can I do this without recompile the linux kernal because I do not have the source code of the linux kernal?

Or can I migrate the VDCE driver?

Where can I find the VDCE driver source or binary?

 

Thanks,

Dongming