This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 WINEC7 boot up issue



Hello Everyone,

     I am trying to boot WINEC7 on DM8148 custom board(though it is similar to EVM8148,only some parts have been additional to this board,rest of the parts have been retained has it is).

Initially the LINUX image was booting fine with the binaries downloaded by EZSDK, i tried running GEL file through CCS on to the DM8148 custom board,after the complete initialization of the gel file, now i am not able to boot through SD card.

I have a question ,while loading GEL file did i corrupt the Boot ROM code from which it is failing to detect the SD card boot switch settings.

If i have corrupted the Boot ROM code, how can i set it to default state.