Hey hi all,
I have downloaded the EZSDK from and when I run the ./setup.sh script it gives as below....
http://www.ti.com/tool/linuxezsdk-sitara
./setup.sh
--------------------------------------------------------------------------------
TISDK setup script
This script will set up your development host for dvsdk development.
Parts of this script require administrator priviliges (sudo access).
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
Verifying Linux host distribution
Ubuntu 10.04 LTS found successfully, continuing..
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will make sure you have the proper host support packages installed
using the following command: sudo apt-get install xinetd tftpd nfs-kernel-server minicom build-essential libncurses5-dev uboot-mkimage autoconf automake
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue
Reading package lists... Done
Building dependency tree
Reading state information... Done
autoconf is already the newest version.
automake is already the newest version.
build-essential is already the newest version.
libncurses5-dev is already the newest version.
nfs-kernel-server is already the newest version.
uboot-mkimage is already the newest version.
xinetd is already the newest version.
minicom is already the newest version.
tftpd is already the newest version.
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.
Package verification and installation successfully completed
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
In which directory do you want to install the target filesystem?(if this directory does not exist it will be created)
[ /usr/local/ti-sdk-am335x-evm/targetNFS ]
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will extract the target filesystem to /usr/local/ti-sdk-am335x-evm/targetNFS
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue
/usr/local/ti-sdk-am335x-evm/targetNFS already exists
(r) rename existing filesystem (o) overwrite existing filesystem (s) skip filesystem extraction
[r]
Path for old filesystem:
[ /usr/local/ti-sdk-am335x-evm/targetNFS.09032012_14.28 ]
Successfully moved old /usr/local/ti-sdk-am335x-evm/targetNFS to /usr/local/ti-sdk-am335x-evm/targetNFS.09032012_14.28
Successfully extracted tisdk-rootfs-am335x-evm.tar.gz to /usr/local/ti-sdk-am335x-evm/targetNFS
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will set up the SDK to install binaries in to:
/usr/local/ti-sdk-am335x-evm/targetNFS/home/root/am335x-evm
The files will be available from /home/root/am335x-evm on the target.
This setting can be changed later by editing Rules.make and changing the
EXEC_DIR or DESTDIR variable (depending on your SDK).
Press return to continue
Rules.make edited successfully..
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will export your target filesystem for NFS access.
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue
/usr/local/ti-sdk-am335x-evm/targetNFS already NFS exported, skipping..
* Stopping NFS kernel daemon [ OK ]
* Unexporting directories for NFS kernel daemon... [ OK ]
* Exporting directories for NFS kernel daemon... [ OK ]
* Starting NFS kernel daemon [ OK ]
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
Which directory do you want to be your tftp root directory?(if this directory does not exist it will be created for you)
[ /tftpboot ]
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will set up the tftp server in the /tftpboot directory.
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue
/tftpboot already exists, not creating..
/tftpboot/uImage-am335x-evm.bin already exists. The existing installed file can be renamed and saved under the new name.
(r) rename (o) overwrite (s) skip copy
[r] o
Successfully overwritten uImage-am335x-evm.bin in tftp root directory /tftpboot
/etc/xinetd.d/tftp already exists..
/tftpboot already exported for TFTP, skipping..
Restarting tftp server
Rather than invoking init scripts through /etc/init.d, use the service(8)
utility, e.g. service xinetd stop
Since the script you are attempting to invoke has been converted to an
Upstart job, you may also use the stop(8) utility, e.g. stop xinetd
xinetd stop/waiting
Rather than invoking init scripts through /etc/init.d, use the service(8)
utility, e.g. service xinetd start
Since the script you are attempting to invoke has been converted to an
Upstart job, you may also use the start(8) utility, e.g. start xinetd
xinetd start/running, process 4431
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will set up minicom (serial communication application) for
SDK development
For boards that contain a USB-to-Serial converter on the board (BeagleBone),
the port used for minicom will be automatically detected. By default Ubuntu
will not recognize this device. Setup will add will add a udev rule to
/etc/udev/ so that from now on it will be recognized as soon as the board is
plugged in.
For other boards, the serial will defualt to /dev/ttyS0. Please update based
on your setup.
--------------------------------------------------------------------------------
NOTE: For boards with a built-in USB to Serial adapter please press
ENTER at the prompt below. The correct port will be determined
automatically at a later step. For all other boards select
the serial port that the board is connected to
Which serial port do you want to use with minicom?
[ /dev/ttyS0 ]
Copied existing /root/.minirc.dfl to /root/.minirc.dfl.old
Configuration saved to /root/.minirc.dfl. You can change it further from inside
minicom, see the Software Development Guide for more information.
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will set up the u-boot variables for booting the EVM.
Becuase the not all AM335x devices have a NAND, the u-boot variables will
be stored in uEnv.txt on the boot partition. U-boot will read this
file on boot.
Autodetected the following ip address of your host, correct it if necessary
[ 10.110.2.146 ]
Select Linux kernel location:
1: TFTP
2: SD card
[ 1 ] 1
Select root file system location:
1: NFS
2: SD card
[ 1 ] 1
Available kernel images in /tftproot:
uImage-am335x-evm.bin
uImage-am335x-evm.bin.09012012_18.31
uImage-am335x-evm.bin.09032012_12.05
Which kernel image do you want to boot from TFTP?
[ uImage-am335x-evm.bin ]
--------------------------------------------------------------------------------
Would you like to create a minicom script with the above parameters (y/n)?
[ y ]
Successfully wrote /usr/local/ti-sdk-am335x-evm/bin/setupBoard.minicom
Would you like to run the setup script now (y/n)? This requires you to connect
the RS-232 cable between your host and EVM as well as your ethernet cable as
described in the Quick Start Guide. Once answering 'y' on the prompt below
you will have 300 seconds to connect the board and power cycle it
before the setup times out
After successfully executing this script, your EVM will be set up. You will be
able to connect to it by executing 'minicom -w' or if you prefer a windows host
you can set up Tera Term as explained in the Software Developer's Guide.
If you connect minicom or Tera Term and power cycle the board Linux will boot.
[ y ]
Welcome to minicom 2.5
OPTIONS: I18n
Compiled on May 2 2011, 00:39:27.
Port /dev/ttyS0
Press CTRL-A Z for help on special keys
bigger 50
and when I terminate the process minicom by ctrl+a+x) it gives like this.... but finally it does not boot the kernel why ??? and it has not set the uboot parameters or it has not done anything regarding uEnv.txt setup ???? Is anything there which has been left to set...???? if anybody have any idea about this then please let me know... thanks
CTRL-A Z for help |115200 8N1 | NOR | Minicom 2.5 | VT102 | Offline
/usr/local/ti-sdk-am335x-evm
You can manually run minicom in the future with this setup script using: minicom -S ./bin/setupBoard.minicom
--------------------------------------------------------------------------------
TISDK setup completed!
Please continue reading the Software Developer's Guide for more information on
how to develop software on the EVM
root@pc:/usr/local/ti-sdk-am335x-evm# minicom -S ./b
bin/ board-support/
root@pc:/usr/local/ti-sdk-am335x-evm# minicom -S ./b
bin/ board-support/
root@pc:/usr/local/ti-sdk-am335x-evm# minicom -S ./bin/setupBoard.minicom
Welcome to minicom 2.5
OPTIONS: I18n
Compiled on May 2 2011, 00:39:27.
Port /dev/ttyS0
Press CTRL-A Z for help on special keys
bigger 50
Regards
Muhammad