Hello I have questions about connecting converters to the OMAPL138. I'm not sure if this is the right forum, and if not please let me know where to post or who to talk to.
1) Can two devices (DAC and ADC) be connected to SPI0 (off of the OMAPL138) and still meet timing requirements? Also do you have any app notes on connecting a SPI DAC and ADC off the same port?
2) We are currently connecting the eval board DAC7654 to the OMAP ref board. Do I need to connect the LOAD and LDAC lines to a GPIO on the OMAP? Or can the DAC function without these two lines?
Thanks,
Rachel