Hello,
I try to use UART1 on DA850 EVM Logic PD board with DaVinci-PSP-SDK-03.22.00.02 .
Uart1 doesn't work.
The strange part is that it works very well with TI_dvsdk_omapl138-evm_04_03_00_06.
I have activated PINMUX support and debug in kernel config and checked that the both pins UART1_TXD and UART1_RXD are disabled.
I have disabled UART1 flow control.
The only difference with a standard system is that I used RMII PHY on UI board in place of MII PHY.
I'm stuuck here.
What are the UART management differences between kernel 2.6.37 and kernel 3.3.
Any idea is welcome
Best regards
Gilbert Brisset.