Hi All,
I'm using the release http://www.omappedia.com/wiki/L27.IS.2.M1_OMAP4_Icecream_Sandwich_Release_Notes.
When i boot the blaze tablet with above release i'm getting the following error's:
[ 6.594940] omapdss DSI error: rx fifo not empty when sending BTA, dumping data:
[ 6.603576] omapdss DSI error: dsi_vc_send_bta channel 1
[ 6.609558] omapdss DSI error: rawval 0x17000202
[ 6.615051] omapdss DSI error: ACK with ERROR (0x2):
[ 6.640472] tc358765 display0: reg read 13c, val=00000004
[ 6.649841] tc358765 display0: reg read 13c, val=00000004
[ 6.687713] tc358765 display0: power_on done
[ 6.695190] omaplfb OMAPLFBInitFBDev: Device 0: Requesting 4 TILER 2D framebuffers
[ 6.706451] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:05:44 UTC (946685144)
[ 6.716979] Freeing init memory: 280K
[ 6.728973] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 6.828369] (stk) :ldisc installation timeout
[ 6.832977] (stk) :ldisc_install = 0
[ 6.843994] sr_class1p5_calib_work: mpu: Calibration complete: Voltage Nominal=1380000Calib=1180000 margin=0
[ 6.923980] EXT4-fs (mmcblk0p8): mounted filesystem with ordered data mode. Opts: (null)
[ 7.389770] omap-rproc omap-rproc.1: Loaded BIOS image ducati-m3.bin, size 5756300
[ 7.398223] omap-rproc omap-rproc.1: BIOS image version is 2
[ 7.425109] omap-iommu omap-iommu.0: iommu_get: ducati qos_request
[ 7.445709] omap_hwmod: ipu: failed to hardreset
[ 7.450836] omap-iommu omap-iommu.0: ducati: version 2.1
[ 7.463134] omap-rproc omap-rproc.1: remote processor ipu is now up
[ 7.476226] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.483093] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.489959] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.496856] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.503845] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x32
[ 7.512329] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x33
[ 7.520629] virtio_rpmsg_bus virtio0: creating channel rpmsg-omx addr 0x3c
[ 7.528289] rpmsg_omx rpmsg-omx0: new OMX connection srv channel: 1024 -> 60!
[ 7.546661] EXT4-fs (mmcblk0p10): recovery complete
[ 7.552703] EXT4-fs (mmcblk0p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
[ 7.580963] EXT4-fs (mmcblk0p9): recovery complete
[ 7.587249] EXT4-fs (mmcblk0p9): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
[ 7.611145] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)
[ 7.663116] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 7.690368] HDCP: failed to load keys
[ 7.825653] usb 1-1.1: USB disconnect, device number 3
[ 7.834930] android_usb: already disabled
[ 7.840148] mtp_bind_config
[ 7.843200] adb_bind_config
[ 7.848358] warning: `adbd' uses 32-bit capabilities (legacy support in use)
[ 7.856353] adb_open
[ 7.892333] virtio_rpmsg_bus virtio1: creating channel rpmsg-omx addr 0x3c
[ 7.902221] rpmsg_omx rpmsg-omx1: new OMX connection srv channel: 1024 -> 60!
[ 7.968139] PVR: Installing MISR with cookie c08b5818
[ 7.976715] PVR: Installing device LISR SGX ISR on IRQ 53 with cookie c790c400
[ 7.985778] PVR: OSUnMapPhysToLin: unmapping 65535 bytes from c8be0000
[ 7.992980] (stk) : timed out waiting for ldisc to be un-installed
[ 8.000579] PVR: SysFinalise: Version string: SGX revision = 1.2.0
shell@android:/ $ [ 8.109436] (stk) :ldisc_install = 1
[ 8.164093] (stc): st_tty_open
[ 8.165283] android_work: sent uevent USB_STATE=CONNECTED
[ 8.169982] android_work: sent uevent USB_STATE=DISCONNECTED
[ 8.183807] (stk) :line discipline installed
[ 8.189514] (stk) :TIInit_10.6.15.bts
[ 8.257293] android_work: sent uevent USB_STATE=CONNECTED
[ 8.264984] android_usb gadget: high speed config #1: android
[ 8.271789] android_work: sent uevent USB_STATE=CONFIGURED
[ 8.592742] (stc): add_channel_to_table: id 2
[ 8.597961] (stc): st_register(3)
[ 8.601654] (stc): add_channel_to_table: id 3
[ 8.607299] (stc): st_register(4)
[ 8.611389] (stc): add_channel_to_table: id 4
[ 8.640960] sr_class1p5_calib_work: mpu: Calibration complete: Voltage Nominal=1317000Calib=1080000 margin=0
[ 8.931060] rpmsg_omx rpmsg-omx1: local addr assigned: 0x401
[ 8.943603] rpmsg_omx rpmsg6: conn rsp: status 0 addr 101
[ 8.984802] sr_class1p5_calib_work: core: Calibration complete: Voltage Nominal=1250000Calib=1038160 margin=13000
[ 9.314575] tc358765 display0: disable
[ 9.314575] misc dsscomp: [c73b7c00] ignoring set failure -22
[ 9.331481] tc358765 display0: enable
[ 9.331481] tc358765 display0: power_on
[ 9.477752] omapdss DSI error: rx fifo not empty when sending BTA, dumping data:
[ 9.477783] omapdss DSI error: dsi_vc_send_bta channel 1
[ 9.477813] omapdss DSI error: rawval 0x17000202
[ 9.477813] omapdss DSI error: ACK with ERROR (0x2):
[ 9.477844] omapdss DSI error: SoT Sync Error
[ 9.492858] tc358765 display0: reg read 13c, val=00000004
[ 9.496337] tc358765 display0: reg read 13c, val=00000004
[ 9.531555] tc358765 display0: power_on done
[ 10.548187] Invalid Device Structure
[ 10.642944] (stc): remove_channel_from_table: id 2
[ 10.648376] (stc): remove_channel_from_table: id 3
[ 10.654083] (stc): remove_channel_from_table: id 4
[ 10.664367] (stc): all chnl_ids unregistered
[ 10.669128] (stk) :ldisc_install = 0
[ 10.673492] (stc): st_tty_close
[ 16.190917] tsl2771_read_als:cdata is NULL
[ 16.197235] tsl2771_read_als:cdata is NULL
[ 19.280670] request_suspend_state: wakeup (3->0) at 19741424563 (2000-01-01 00:05:57.065582276 UTC)
[ 24.140838] omap-rproc omap-rproc.1: rproc_watchdog_isr
[ 24.147186] omap_rproc_dump_registers: REGISTER DUMP FOR REMOTEPROC ipu
[ 24.154663] omap_rproc_dump_registers: PC is at 0033c942
[ 24.160827] omap_rproc_dump_registers: LR is at 0025104b
[ 24.167114] omap_rproc_dump_registers: pc : [<0033c942>] lr : [<0025104b>] psr: 61000000
[ 24.167114] sp : 8511b920 ip : 8524a0fe fp : 8514ef28
[ 24.182830] omap_rproc_dump_registers: r10: 00000000 r9 : 0025120c r8 : 85111b24
[ 24.191162] omap_rproc_dump_registers: r7 : 00000001 r6 : 8511b9bc r5 : 851116e4 r4 : 8514ef70
[ 24.201019] omap_rproc_dump_registers: r3 : 852672f0 r2 : 8511b938 r1 : 00000006 r0 : 00000000
[ 24.210845] omap_rproc_dump_registers: Flags: nZCv IRQs on FIQs on
[ 24.218139] _event_notify: remoteproc: ipu has crashed
[ 24.223785] rpmsg_rproc_error: Fatal error in ipu
[ 24.229125] rpmsg_rproc_error: Fatal error in ipu
[ 24.234405] rpmsg_reset_work: reseting virtio device 0
[ 24.240173] rpmsg_resmgr rpmsg0: Enter rprm_remove
[ 24.247070] rpmsg_omx rpmsg-omx0: rpmsg omx driver is removed
[ 24.254425] rpmsg_reset_work: reseting virtio device 1
[ 24.260131] rpmsg_resmgr rpmsg2: Enter rprm_remove
[ 24.265869] rpmsg_omx rpmsg-omx1: rpmsg omx driver is removed
[ 24.274047] rproc_reset_poolmem: invalid pool
[ 24.279144] omap-rproc omap-rproc.1: stopped remote processor ipu
[ 24.286987] omap-rproc omap-rproc.1: powering up ipu
[ 24.293975] virtio_rpmsg_bus virtio2: rpmsg backend virtproc probed successfully
[ 24.307525] virtio_rpmsg_bus virtio3: rpmsg backend virtproc probed successfully
[ 24.337860] omap-rproc omap-rproc.1: Loaded BIOS image ducati-m3.bin, size 5756300
[ 24.346374] omap-rproc omap-rproc.1: BIOS image version is 2
[ 24.372497] omap-iommu omap-iommu.0: iommu_get: ducati qos_request
[ 24.393249] omap_hwmod: ipu: failed to hardreset
[ 24.398498] omap-iommu omap-iommu.0: ducati: version 2.1
[ 24.410858] omap-rproc omap-rproc.1: remote processor ipu is now up
[ 24.424072] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 24.434936] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 24.442932] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 24.449768] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 24.456542] virtio_rpmsg_bus virtio2: creating channel rpmsg-client-sample addr 0x32
[ 24.465270] virtio_rpmsg_bus virtio2: creating channel rpmsg-client-sample addr 0x33
[ 24.473876] virtio_rpmsg_bus virtio2: creating channel rpmsg-omx addr 0x3c
[ 24.481933] rpmsg_omx rpmsg-omx0: new OMX connection srv channel: 1024 -> 60!
[ 24.846588] virtio_rpmsg_bus virtio3: creating channel rpmsg-omx addr 0x3c
[ 24.856658] rpmsg_omx rpmsg-omx1: new OMX connection srv channel: 1024 -> 60!
[ 25.191497] acc_open
[ 25.194213] acc_release
[ 26.484039] mtp_open
but tablet booted successfully.
And when i opened the camera app I'm getting the following error:
[ 34.958709] rpmsg_omx rpmsg-omx1: local addr assigned: 0x401
[ 34.968139] omap-iommu omap-iommu.0: iommu_get: ducati qos_request
[ 34.989532] omap_hwmod: ipu: failed to hardreset
[ 34.998077] omap-iommu omap-iommu.0: ducati: version 2.1
[ 35.132110] rpmsg_omx rpmsg13: conn rsp: status 0 addr 101
[ 37.511016] rpmsg_omx rpmsg-omx1: Disconnecting from OMX service at 101
Please can someone suggest me a solution to this.
Thanks in advance
Regards,
Naresh k