The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C665x ADC connection via uPP

Other Parts Discussed in Thread: ADS8471, OMAP-L138, ADS5560

I would like to know whether there is the ADC which can connect directly to uPP.

Here is a way to connect ADS8471 to OMAP-L138 via uPP.

http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/144344.aspx

A BUSY pin of ADS8471 is tied to a CHx_CLK pin of OMAP-L138. I guess that it does not meet the setup time.

Is not there the ADC which can connect directly to uPP?

Best regards,

Daisuke