This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C problem while inserting VPSS module in DM8148 EVM

Hi,

I am using the DM8148 EVM. After I start the board with the original SD card which came with the board, and take a dmesg log, I found that vpss module insertion which is done through load-hd-firmware.sh is giving the following error message while inserting.

VPSS_CAPTURE: cap init
omap_i2c omap_i2c.3: controller timed out
I2C: Transfer failed at vps_ti814x_select_video_decoder 188 with error code: -110

In the  load-hd-firmware.sh script in line no. 33  the following command is responsible for inserting the vpss module

"    modprobe vpss sbufaddr=0xBFB00000 mode=hdmi:1080p-60 debug=1 "


I have attached the full dmesg log. The error can be found in line no. 607 of the dmesg logs.

root@dm814x-evm:~# dmesg
Linux version 2.6.37 (root@ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Sun Feb 2 15:15:45 IST 2014
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 2.1
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
On node 0 totalpages: 162304
free_area_init_node: node 0, pgdat c056fd98, node_mem_map c05af000
  Normal zone: 728 pages used for memmap
  Normal zone: 0 pages reserved
  Normal zone: 92456 pages, LIFO batch:31
  HighMem zone: 928 pages used for memmap
  HighMem zone: 68192 pages, LIFO batch:15
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 160648
Kernel command line: console=ttyO0,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M  notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 364MB 270MB = 634MB total
Memory: 637476k/637476k available, 62940k reserved, 276480K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    vmalloc : 0xd7000000 - 0xf8000000   ( 528 MB)
    lowmem  : 0xc0000000 - 0xd6c00000   ( 364 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .init : 0xc0008000 - 0xc003c000   ( 208 kB)
      .text : 0xc003c000 - 0xc0525000   (5028 kB)
      .data : 0xc0526000 - 0xc0571780   ( 302 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
PM: Adding info for No Bus:platform
omap_voltage_early_init: voltage driver support not added
PM: Adding info for No Bus:omap
regulator: core version 0.5
PM: Adding info for platform:reg-dummy
PM: Adding info for No Bus:regulator.0
regulator: dummy:
NET: Registered protocol family 16
PM: Adding info for platform:mpu.0
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
PM: Adding info for platform:l3_slow.0
PM: Adding info for platform:omap_gpio.0
PM: Adding info for platform:omap_gpio.1
PM: Adding info for platform:omap_gpio.2
PM: Adding info for platform:omap_gpio.3
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
PM: Adding info for No Bus:vtcon0
omap_mux_init: Add partition: #1: core, flags: 4
PM: Adding info for platform:omap_uart.0
PM: Adding info for platform:omap_uart.1
PM: Adding info for platform:omap_uart.2
PM: Adding info for platform:omap_uart.3
PM: Adding info for platform:omap_uart.4
PM: Adding info for platform:omap_uart.5
PM: Adding info for platform:omap_i2c.1
PM: Adding info for platform:omap_i2c.3
PM: Adding info for platform:davinci-mcasp.2
PM: Adding info for platform:mmci-omap-hs.0
PM: Adding info for platform:omap2-nand.0
PM: Adding info for platform:ti81xx-usbss
NOR: Can't request GPMC CS
PM: Adding info for platform:omap-mailbox
PM: Adding info for platform:omap2_mcspi.1
PM: Adding info for platform:omap2_mcspi.2
PM: Adding info for platform:omap2_mcspi.3
PM: Adding info for platform:omap2_mcspi.4
PM: Adding info for platform:omap2_elm.1
PM: Adding info for platform:arm-pmu.0
PM: Adding info for platform:davinci_mdio.0
PM: Adding info for platform:cpsw.0
PM: Adding info for platform:ti81xx_pcie.0
PM: Adding info for platform:edma
PM: Adding info for platform:davinci-pcm-audio
PM: Adding info for platform:d_can
PM: Adding info for platform:ahci.0
PM: Adding info for platform:omap_rtc
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
PM: Adding info for platform:vpss
registered ti81xx_vpss device
PM: Adding info for platform:t81xx_vidout
registered ti81xx_vidout device
PM: Adding info for platform:TI81XX_HDMI
registered ti81xx on-chip HDMI device
PM: Adding info for platform:ti81xxfb
registered ti81xx_fb device
PM: Adding info for platform:ti81xxvin
registered ti81xx_vin device
PM: Adding info for platform:omap_wdt
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd7020000
ti81xx_pcie: Starting PCI scan...
PM: Adding info for No Bus:pci0000:00
PM: Adding info for No Bus:0000:00
PCI: bus0: Fast back to back transfers enabled
pci_bus 0000:00: resource 0 [mem 0x20000000-0x2fffffff]
pci_bus 0000:00: resource 1 [io  0x40000000-0x402fffff]
PM: Adding info for No Bus:default
bio: create slab <bio-0> at 0
PM: Adding info for No Bus:vga_arbiter
vgaarb: loaded
SCSI subsystem initialized
libata version 3.00 loaded.
PM: Adding info for No Bus:spi1
PM: Adding info for spi:spi1.0
PM: Adding info for No Bus:spi2
PM: Adding info for No Bus:spi3
PM: Adding info for No Bus:spi4
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea2080b
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
PM: Adding info for platform:musb-hdrc.0
PM: Adding info for platform:musb-hdrc.1
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
PM: Adding info for i2c:i2c-1
PM: Adding info for i2c:1-0050
PM: Adding info for i2c:1-0023
PM: Adding info for i2c:1-0018
PM: Adding info for i2c:1-0020
PM: Adding info for i2c:1-0040
PM: Adding info for i2c:1-0021
pcf857x 1-0021: gpios 128..143 on a pcf8575
PM: Adding info for i2c:1-004a
PM: Adding info for i2c:1-002d
PM: Adding info for platform:tps65910-pmic
PM: Adding info for No Bus:regulator.1
regulator: VRTC: 1800 mV
PM: Adding info for No Bus:regulator.2
regulator: VIO: 1500 mV
PM: Adding info for No Bus:regulator.3
regulator: VDD1: 600 <--> 1500 mV at 1200 mV
PM: Adding info for No Bus:regulator.4
regulator: VDD2: 600 <--> 1500 mV at 1200 mV
PM: Adding info for No Bus:regulator.5
regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV
PM: Adding info for No Bus:regulator.6
regulator: LDO1: 1100 <--> 3300 mV at 1800 mV
PM: Adding info for No Bus:regulator.7
regulator: LDO2: 1100 <--> 3300 mV at 1800 mV
PM: Adding info for No Bus:regulator.8
regulator: LDO3: 1100 <--> 3300 mV at 3300 mV
PM: Adding info for No Bus:regulator.9
regulator: LDO4: 1100 <--> 3300 mV at 1800 mV
PM: Adding info for No Bus:regulator.10
regulator: LDO5: 1100 <--> 3300 mV at 3300 mV
PM: Adding info for No Bus:regulator.11
regulator: LDO6: 1100 <--> 3300 mV at 3300 mV
PM: Adding info for No Bus:regulator.12
regulator: LDO7: 1100 <--> 3300 mV at 3300 mV
PM: Adding info for No Bus:regulator.13
regulator: LDO8: 1100 <--> 3300 mV at 1800 mV
PM: Adding info for platform:tps65910-rtc
PM: Adding info for platform:tps65910-power
tps65910 1-002d: No interrupt support, no core IRQ
omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
PM: Adding info for i2c:i2c-3
PM: Adding info for i2c:3-0021
Advanced Linux Sound Architecture Driver Version 1.0.23.
PM: Adding info for No Bus:lo
Switching to clocksource gp timer
PM: Adding info for No Bus:mem
PM: Adding info for No Bus:kmem
PM: Adding info for No Bus:null
PM: Adding info for No Bus:port
PM: Adding info for No Bus:zero
PM: Adding info for No Bus:full
PM: Adding info for No Bus:random
PM: Adding info for No Bus:urandom
PM: Adding info for No Bus:kmsg
PM: Adding info for No Bus:tty
PM: Adding info for No Bus:console
PM: Adding info for No Bus:tty0
PM: Adding info for No Bus:vcs
PM: Adding info for No Bus:vcsa
PM: Adding info for No Bus:vcs1
PM: Adding info for No Bus:vcsa1
PM: Adding info for No Bus:tty1
PM: Adding info for No Bus:tty2
PM: Adding info for No Bus:tty3
PM: Adding info for No Bus:tty4
PM: Adding info for No Bus:tty5
PM: Adding info for No Bus:tty6
PM: Adding info for No Bus:tty7
PM: Adding info for No Bus:tty8
PM: Adding info for No Bus:tty9
PM: Adding info for No Bus:tty10
PM: Adding info for No Bus:tty11
PM: Adding info for No Bus:tty12
PM: Adding info for No Bus:tty13
PM: Adding info for No Bus:tty14
PM: Adding info for No Bus:tty15
PM: Adding info for No Bus:tty16
PM: Adding info for No Bus:tty17
PM: Adding info for No Bus:tty18
PM: Adding info for No Bus:tty19
PM: Adding info for No Bus:tty20
PM: Adding info for No Bus:tty21
PM: Adding info for No Bus:tty22
PM: Adding info for No Bus:tty23
PM: Adding info for No Bus:tty24
PM: Adding info for No Bus:tty25
PM: Adding info for No Bus:tty26
PM: Adding info for No Bus:tty27
PM: Adding info for No Bus:tty28
PM: Adding info for No Bus:tty29
PM: Adding info for No Bus:tty30
PM: Adding info for No Bus:tty31
PM: Adding info for No Bus:tty32
PM: Adding info for No Bus:tty33
PM: Adding info for No Bus:tty34
PM: Adding info for No Bus:tty35
PM: Adding info for No Bus:tty36
PM: Adding info for No Bus:tty37
PM: Adding info for No Bus:tty38
PM: Adding info for No Bus:tty39
PM: Adding info for No Bus:tty40
PM: Adding info for No Bus:tty41
PM: Adding info for No Bus:tty42
PM: Adding info for No Bus:tty43
PM: Adding info for No Bus:tty44
PM: Adding info for No Bus:tty45
PM: Adding info for No Bus:tty46
PM: Adding info for No Bus:tty47
PM: Adding info for No Bus:tty48
PM: Adding info for No Bus:tty49
PM: Adding info for No Bus:tty50
PM: Adding info for No Bus:tty51
PM: Adding info for No Bus:tty52
PM: Adding info for No Bus:tty53
PM: Adding info for No Bus:tty54
PM: Adding info for No Bus:tty55
PM: Adding info for No Bus:tty56
PM: Adding info for No Bus:tty57
PM: Adding info for No Bus:tty58
PM: Adding info for No Bus:tty59
PM: Adding info for No Bus:tty60
PM: Adding info for No Bus:tty61
PM: Adding info for No Bus:tty62
PM: Adding info for No Bus:tty63
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
PM: Adding info for platform:nop_usb_xceiv.0
MUSB controller-0 revision 4ea20800
TxFifo Empty intr disabled
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
PM: Adding info for usb:usb1
PM: Adding info for usb:1-0:1.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
PM: Adding info for No Bus:ep_81
PM: Adding info for No Bus:usbdev1.1
PM: Adding info for No Bus:ep_00
musb-hdrc musb-hdrc.0: USB Host mode controller at d701e000 using DMA, IRQ 18
Registered /proc/driver/musb_hdrc.0
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
PM: Adding info for platform:nop_usb_xceiv.1
MUSB controller-1 revision 4ea20800
TxFifo Empty intr disabled
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
PM: Adding info for usb:usb2
PM: Adding info for usb:2-0:1.0
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
PM: Adding info for No Bus:ep_81
PM: Adding info for No Bus:usbdev2.1
PM: Adding info for No Bus:ep_00
musb-hdrc musb-hdrc.1: USB Host mode controller at d7026800 using DMA, IRQ 19
Registered /proc/driver/musb_hdrc.1
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PCI: CLS 0 bytes, default 64
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
PM: Adding info for No Bus:mailbox-dsp
PM: Adding info for No Bus:mailbox-video
PM: Adding info for No Bus:mailbox-vpss
PM: Adding info for platform:omap-iommu.0
PM: Adding info for platform:omap-iommu.1
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 705
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
PM: Adding info for No Bus:ptmx
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
PM: Adding info for platform:serial8250
PM: Adding info for No Bus:ttyS0
PM: Adding info for No Bus:ttyS1
PM: Adding info for No Bus:ttyS2
PM: Adding info for No Bus:ttyS3
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
PM: Adding info for No Bus:ttyO0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
PM: Adding info for No Bus:ttyO1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
PM: Adding info for No Bus:ttyO2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
PM: Adding info for No Bus:ttyO3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
PM: Adding info for No Bus:ttyO4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
PM: Adding info for No Bus:ttyO5
PM: Adding info for No Bus:1:0
PM: Adding info for No Bus:ram0
PM: Adding info for No Bus:1:1
PM: Adding info for No Bus:ram1
PM: Adding info for No Bus:1:2
PM: Adding info for No Bus:ram2
PM: Adding info for No Bus:1:3
PM: Adding info for No Bus:ram3
PM: Adding info for No Bus:1:4
PM: Adding info for No Bus:ram4
PM: Adding info for No Bus:1:5
PM: Adding info for No Bus:ram5
PM: Adding info for No Bus:1:6
PM: Adding info for No Bus:ram6
PM: Adding info for No Bus:1:7
PM: Adding info for No Bus:ram7
PM: Adding info for No Bus:1:8
PM: Adding info for No Bus:ram8
PM: Adding info for No Bus:1:9
PM: Adding info for No Bus:ram9
PM: Adding info for No Bus:1:10
PM: Adding info for No Bus:ram10
PM: Adding info for No Bus:1:11
PM: Adding info for No Bus:ram11
PM: Adding info for No Bus:1:12
PM: Adding info for No Bus:ram12
PM: Adding info for No Bus:1:13
PM: Adding info for No Bus:ram13
PM: Adding info for No Bus:1:14
PM: Adding info for No Bus:ram14
PM: Adding info for No Bus:1:15
PM: Adding info for No Bus:ram15
brd: module loaded
PM: Adding info for No Bus:7:0
PM: Adding info for No Bus:loop0
PM: Adding info for No Bus:7:1
PM: Adding info for No Bus:loop1
PM: Adding info for No Bus:7:2
PM: Adding info for No Bus:loop2
PM: Adding info for No Bus:7:3
PM: Adding info for No Bus:loop3
PM: Adding info for No Bus:7:4
PM: Adding info for No Bus:loop4
PM: Adding info for No Bus:7:5
PM: Adding info for No Bus:loop5
PM: Adding info for No Bus:7:6
PM: Adding info for No Bus:loop6
PM: Adding info for No Bus:7:7
PM: Adding info for No Bus:loop7
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
PM: Adding info for No Bus:ata1
PM: Adding info for No Bus:ata1
PM: Adding info for No Bus:link1
PM: Adding info for No Bus:link1
PM: Adding info for No Bus:dev1.0
PM: Adding info for No Bus:dev1.0
scsi0 : ahci_platform
PM: Adding info for scsi:host0
PM: Adding info for No Bus:host0
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
PM: Adding info for No Bus:mtd-unmap
PM: Adding info for No Bus:mtd-romap
PM: Adding info for No Bus:mtd-rwmap
omap2-nand driver initializing
No NAND device found.
No NAND device found.
PM: Adding info for No Bus:ubi_ctrl
PM: Adding info for No Bus:0
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffc
PM: Adding info for mdio_bus:0:00
PM: Adding info for mdio_bus:0:01
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
PM: Adding info for No Bus:can0
d_can d_can: d_can device registered (irq=52, irq_obj=53)
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
PM: Adding info for No Bus:mice
mice: PS/2 mouse device common for all mice
ata1: SATA link down (SStatus 0 SControl 300)
qt602240_ts 1-004a: Family ID: 128 Variant ID: 1 Version: 22 Build: 171
qt602240_ts 1-004a: Matrix X Size: 18 Matrix Y Size: 12 Object Num: 17
PM: Adding info for No Bus:input0
input: AT42QT602240/ATMXT224 Touchscreen as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/input/input0
PM: Adding info for No Bus:mouse0
PM: Adding info for No Bus:event0
PM: Adding info for No Bus:rtc0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
PM: Adding info for No Bus:i2c-1
PM: Adding info for No Bus:i2c-3
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
PM: Adding info for No Bus:watchdog
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
PM: Adding info for No Bus:mmc0
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbf900000
PM: Adding info for No Bus:timer
usbcore: registered new interface driver snd-usb-audio
PM: Adding info for platform:soc-audio.0
PM: Adding info for No Bus:TLV320AIC3X
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
PM: Adding info for No Bus:card0
PM: Adding info for No Bus:pcmC0D0p
PM: Adding info for No Bus:pcmC0D0c
PM: Adding info for No Bus:controlC0
ALSA device list:
  #0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
PM: Adding info for No Bus:cpu_dma_latency
PM: Adding info for No Bus:network_latency
PM: Adding info for No Bus:network_throughput
Detected MACID=0:18:32:60:bd:74
PM: Adding info for No Bus:eth0
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
Waiting for root device /dev/mmcblk0p2...
mmc0: new high speed SDHC card at address e624
PM: Adding info for mmc:mmc0:e624
mmcblk0: mmc0:e624 SU08G 7.40 GiB
PM: Adding info for No Bus:179:0
PM: Adding info for No Bus:mmcblk0
 mmcblk0: p1 p2
PM: Adding info for No Bus:mmcblk0p1
PM: Adding info for No Bus:mmcblk0p2
EXT3-fs: barriers not enabled
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 208K
PM: Adding info for No Bus:vcs2
PM: Adding info for No Bus:vcsa2
PM: Removing info for No Bus:vcs2
PM: Removing info for No Bus:vcsa2
udevd (73): /proc/73/oom_adj is deprecated, please use /proc/73/oom_score_adj instead.
NET: Registered protocol family 10

CPSW phy found : id is : 0x4dd074

CPSW phy found : id is : 0x4dd074
ADDRCONF(NETDEV_UP): eth0: link is not ready
PHY: 0:01 - Link is Up - 0/Half
PHY: 0:01 - Link is Down
SysLink version : 2.20.02.20
SysLink module created on Date:Feb  2 2014 Time:15:17:53
PM: Adding info for No Bus:syslinkipc_Osal
PM: Adding info for No Bus:syslinkipc_Ipc
PM: Adding info for No Bus:syslinkipc_ProcMgr
PM: Adding info for No Bus:syslinkipc_Notify
PM: Adding info for No Bus:syslinkipc_MultiProc
PM: Adding info for No Bus:syslinkipc_NameServer
PM: Adding info for No Bus:syslinkipc_SharedRegion
PM: Adding info for No Bus:syslinkipc_HeapBufMP
PM: Adding info for No Bus:syslinkipc_HeapMemMP
PM: Adding info for No Bus:syslinkipc_ListMP
PM: Adding info for No Bus:syslinkipc_GateMP
PM: Adding info for No Bus:syslinkipc_MessageQ
PM: Adding info for No Bus:syslinkipc_SyslinkMemMgr
PM: Adding info for No Bus:syslinkipc_ClientNotifyMgr
PM: Adding info for No Bus:syslinkipc_FrameQBufMgr
PM: Adding info for No Bus:syslinkipc_FrameQ
PM: Adding info for No Bus:syslinkipc_RingIO
PM: Adding info for No Bus:syslinkipc_RingIOShm
VPSS_CORE : core init
VPSS_CORE : cpu version 0x81400281
VPSS_SHRBUF: sbuf init
VPSS_SHRBUF: map 0xbfb00000 to 0xe9c00000 with size 2097152
VPSS_FVID2: fvid2 init
VPSS_FVID2: Handshake...
VPSS_SHRBUF: FOUND 0xbfb00000, end 0xbfd00000, map vir 0xe9c00000 size 4096
VPSS_SHRBUF: free mem paddr 0xbfb00000 vaddr 0xe9c00000 size 4096
VPSS_FVID2: M3 firmware version 0x1000145 is newer,driver may not work properly.
VPSS_SYSTEM: enter system init
VPSS_SHRBUF: FOUND 0xbfb00000, end 0xbfd00000, map vir 0xe9c00000 size 4096
VPSS_SHRBUF: FOUND 0xbfb01000, end 0xbfd00000, map vir 0xe9c01000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f20328c with notifyno 10 within 3 ms
VPSS_FVID2: send control with cmd 0x10080002
VPSS_FVID2: control event 0x10080002 return 0 within 0 ms.
VPSS_DCTRL: dctrl init
VPSS_SHRBUF: FOUND 0xbfb02000, end 0xbfd00000, map vir 0xe9c02000 size 4096
VPSS_SHRBUF: FOUND 0xbfb03000, end 0xbfd00000, map vir 0xe9c03000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032ac with notifyno 11 within 0 ms
VPSS_DCTRL: mode hdmi:1080p-60
VPSS_FVID2: send control with cmd 0x10040003
VPSS_FVID2: control event 0x10040003 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040003
VPSS_FVID2: control event 0x10040003 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040003
VPSS_FVID2: control event 0x10040003 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001c
VPSS_FVID2: control event 0x1004001c return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001c
VPSS_FVID2: control event 0x1004001c return 0 within 0 ms.
VPSS_SYSTEM: enter set pll 148500KHz for VENC 2
VPSS_SYSTEM: request clk 1485000000Hz
VPSS_SYSTEM: enter set pll 148500KHz for VENC 1
VPSS_SYSTEM: request clk 1485000000Hz
VPSS_SYSTEM: enter set pll 54000KHz for VENC 0
VPSS_SYSTEM: request clk 1080000000Hz
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040019
VPSS_FVID2: control event 0x10040019 return 0 within 0 ms.
VPSS_GRPX : grpx init
VPSS_SHRBUF: FOUND 0xbfb04000, end 0xbfd00000, map vir 0xe9c04000 size 4096
VPSS_VIDEO: video init
VPSS_SHRBUF: FOUND 0xbfb05000, end 0xbfd00000, map vir 0xe9c05000 size 8192
VPSS_CAPTURE: cap init
omap_i2c omap_i2c.3: controller timed out
I2C: Transfer failed at vps_ti814x_select_video_decoder 188 with error code: -110
VPSS_SHRBUF: FOUND 0xbfb07000, end 0xbfd00000, map vir 0xe9c07000 size 49152
VPSS_SHRBUF: sharing buffer used 77824 byte, left 2019328 bytes
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 1 ms.
VPSS_GRPX : (1)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 3 ms.
VPSS_GRPX : (2)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- get sc params.
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (1)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (1)- get region params.
VPSS_GRPX : (1)- get sc params.
VPSS_GRPX : (1)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (1) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (2)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (2)- get region params.
VPSS_GRPX : (2)- get sc params.
VPSS_GRPX : (2)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (2) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_GRPX : (0)- set format bpp 32 df 4104, pitch 7680.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- set region params.
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_GRPX : (1)- apply changes into FVID2_FRAME.
VPSS_GRPX : (1)- set format bpp 32 df 4104, pitch 7680.
VPSS_GRPX : (1)- get region params.
VPSS_GRPX : (1)- set region params.
VPSS_GRPX : (1)- add buffer 0xb2200000
VPSS_GRPX : (1)- apply changes into FVID2_FRAME.
VPSS_GRPX : (2)- apply changes into FVID2_FRAME.
VPSS_GRPX : (2)- set format bpp 32 df 4104, pitch 2880.
VPSS_GRPX : (2)- get region params.
VPSS_GRPX : (2)- set region params.
VPSS_GRPX : (2)- add buffer 0xb3200000
VPSS_GRPX : (2)- apply changes into FVID2_FRAME.
PM: Adding info for No Bus:fb0
PM: Adding info for No Bus:fb1
PM: Adding info for No Bus:fb2
VPSS_GRPX : (0)- s: 19 e:24 vid:4
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_DCTRL: node already disconnected
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_GRPX : (0)- numedge :1
VPSS_DCTRL: enter venc disable
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001b
VPSS_FVID2: control event 0x1004001b return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_SYSTEM: enter set pll 33500KHz for VENC 1
VPSS_SYSTEM: request clk 1340000000Hz
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040004
VPSS_FVID2: control event 0x10040004 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040003
VPSS_FVID2: control event 0x10040003 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040019
VPSS_FVID2: control event 0x10040019 return 0 within 0 ms.
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_DCTRL: node already connected
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- set input 800 x 480 P:1.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 49 ms.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- get sc params.
VPSS_GRPX : (0) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- set format bpp 32 df 4104, pitch 3200.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_GRPX : (0)- set clut 0x95f0c000
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_GRPX : stop grpx0
VPSS_FVID2: send control with cmd 0x00000006
VPSS_FVID2: control event 0x6 return 0 within 65 ms.
VPSS_GRPX : delete GRPX0
VPSS_FVID2: enter delete.
VPSS_FVID2: delete event return 0 within 0 ms
VPSS_SHRBUF: free mem paddr 0xbfb13000 vaddr 0xe9c13000 size 4096
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
HDMI W1 rev 4.0
HDMI CEC Spec version 1.2
PM: Adding info for No Bus:TI81XX_HDMI
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040004
VPSS_FVID2: control event 0x10040004 return 0 within 0 ms.
VPSS_SYSTEM: enter set pll 148500KHz for VENC 3
VPSS_SYSTEM: request clk 1485000000Hz
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 1
hdmi: *** Set PHY power mode to 2
I2C No Ack

hdmi: Enter HDMI_W1_GlobalInitVars()
hdmi: Enter HDMI_Core_GlobalInitVars()
hdmi: Enter HDMI_W1_ConfigVideoResolutionTiming()
hdmi: Enter HDMI_W1_ConfigVideoInterface()
hdmi: HDMI_WP_AUDIO_CFG = 0x1030006
hdmi: HDMI_WP_AUDIO_CFG2 = 0x20c0
hdmi: HDMI_WP_AUDIO_CTRL = 0x20
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter DSS_HDMI_CORE_POWER_DOWN_DISABLE()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_RELEASE()
hdmi: Enter HDMI_W1_StartVideoFrame  ()
hdmi: Irqenable 60000011
hdmi: 40 hpd
PM: Adding info for No Bus:tlc59108-bl
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 42 ms.
VPSS_GRPX : stop grpx0
VPSS_FVID2: send control with cmd 0x00000006
VPSS_FVID2: control event 0x6 return 0 within 66 ms.
VPSS_GRPX : delete GRPX0
VPSS_FVID2: enter delete.
VPSS_FVID2: delete event return 0 within 0 ms
VPSS_SHRBUF: free mem paddr 0xbfb13000 vaddr 0xe9c13000 size 4096
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 50 ms.
VPSS_GRPX : stop grpx0
VPSS_FVID2: send control with cmd 0x00000006
VPSS_FVID2: control event 0x6 return 0 within 66 ms.
VPSS_GRPX : delete GRPX0
VPSS_FVID2: enter delete.
VPSS_FVID2: delete event return 0 within 0 ms
VPSS_SHRBUF: free mem paddr 0xbfb13000 vaddr 0xe9c13000 size 4096
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 46 ms.
VPSS_GRPX : stop grpx0
VPSS_FVID2: send control with cmd 0x00000006
VPSS_FVID2: control event 0x6 return 0 within 65 ms.
VPSS_GRPX : delete GRPX0
VPSS_FVID2: enter delete.
VPSS_FVID2: delete event return 0 within 0 ms
VPSS_SHRBUF: free mem paddr 0xbfb13000 vaddr 0xe9c13000 size 4096
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 50 ms.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- get sc params.
VPSS_GRPX : (0) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- set format bpp 32 df 4104, pitch 3200.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_GRPX : stop grpx0
VPSS_FVID2: send control with cmd 0x00000006
VPSS_FVID2: control event 0x6 return 0 within 65 ms.
VPSS_GRPX : delete GRPX0
VPSS_FVID2: enter delete.
VPSS_FVID2: delete event return 0 within 0 ms
VPSS_SHRBUF: free mem paddr 0xbfb13000 vaddr 0xe9c13000 size 4096
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 53 ms.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- get sc params.
VPSS_GRPX : (0) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- set format bpp 32 df 4104, pitch 3200.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_GRPX : stop grpx0
VPSS_FVID2: send control with cmd 0x00000006
VPSS_FVID2: control event 0x6 return 0 within 65 ms.
VPSS_GRPX : delete GRPX0
VPSS_FVID2: enter delete.
VPSS_FVID2: delete event return 0 within 0 ms
VPSS_SHRBUF: free mem paddr 0xbfb13000 vaddr 0xe9c13000 size 4096
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
PM: Adding info for platform:pvrsrvkm
PM: Adding info for No Bus:pvrsrvkm
VPSS_GRPX : create grpx0
VPSS_DCTRL: enter set node
VPSS_FVID2: send control with cmd 0x10040018
VPSS_FVID2: control event 0x10040018 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040017
VPSS_FVID2: control event 0x10040017 return 0 within 0 ms.
VPSS_SHRBUF: FOUND 0xbfb13000, end 0xbfd00000, map vir 0xe9c13000 size 4096
VPSS_FVID2: Fvid2 handle 0x9f2032cc with notifyno 12 within 0 ms
VPSS_GRPX : (0)- add buffer 0xb0a00000
VPSS_GRPX : start grpx0
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000003
VPSS_FVID2: control event 0x3 return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10000002
VPSS_FVID2: control event 0x10000002 return 0 within 0 ms.
VPSS_FVID2: queue event return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x00000005
VPSS_FVID2: control event 0x5 return 0 within 60 ms.
PM: Adding info for No Bus:bccat0
VPSS_GRPX : start grpx0

Thanks,

Debasish