Hi
I had a question about 138 SDK.
There are two SDK: OMAP-L138 LCDK and Experimenter Kit, right?
What's difference about that?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Changsheng Li,
Here are some of the hardware differences we matched with respect to two boards
|
Hardware |
Logic PD OMAP-L138 Experimenter Kit |
OMAP-L138 LCDK Board |
Remarks |
|
Processor |
OMAP-L138 dual core, C6748 VLIW DSP and ARM926 RISC GPP on a SOM configuration |
OMAP-L138 dual core or C6748 VLIW DSP and ARM926 RISC GPP- soldered on board |
|
|
DDR |
128 MB mDDR SDRAM* |
128 MB DDR2 SDRAM |
|
|
Flash |
8 MB SPI NOR Flash |
128 MB NAND Flash |
|
|
Ethernet |
One RJ45 Ethernet jack connector with magnetics (application/debug) |
One Fast Ethernet Port (10/100 Mbps) with status LEDs
|
|
|
RS232 |
115.2kbps RS-232 debug serial port |
One mini-USB Serial Port (on-board serial to USB)
|
|
|
USB |
|
|
|
|
Audio |
TLV320AIC3106 (access to line in and line out only) |
TLV320AIC3106 Three Audio Ports (1 LINE IN & 1 LINE OUT & 1 MIC IN)
|
LCDK have microphone -IN support |
|
Display |
Integrated (LCD, touch, and backlight) Connector for optional Zoom Display Kits |
LCD Port (Beagle board XM connectors) |
|
|
Video |
Need to have a separate Logic PD User Interface (UI) Board |
Composite Video (NTSC/PAL) input & VGA output, |
Need UI board for OMAP-L138 to have this feature |
|
Camera Interface |
Need to have a separate Logic PD User Interface (UI) Board |
One Leopard Imaging Camera Sensor Input (36-pin ZIP connector)
|
Need UI board for OMAP-L138 to have this feature |
|
SATA |
1 - Serial ATA connector (3 Gbps) |
1 -Serial ATA connector (3 Gbps) |
|
|
MMC/SD |
One MMC/SD card slot |
1-Micro SD/MMC Slot |
|
|
eHRPWM |
eHRPWM1 Signals brought out via J30 connector |
eHRPWM1 Signals brought out via J15 connector |
|
|
uPP (Universal Parallel Port) |
NIL |
NIL |
|
|
UHPI |
NIL |
NIL |
|
|
SPI |
SPI0 Signal brought out via J28 Connector board |
Signal brought out via J15 Connector |
|
|
I2C |
I2C0 Signal brought out via J28 Connector base board |
I2C0 Signal brought out via J15 Connector |
|
|
eCAP |
eCAP0, eCAP1& eCAP2 Signals brought out via J30 Audio Connector |
Two ECAP1_APWM2 &ECAP2_APWM2 Signals brought out via J15 Connector |
|
|
Timer |
Timer 0&1 Signals brought out via J29 Connector |
Timer 2&3 Signals brought out via J15 Connector |
|
|
GPIO |
Signals Brought out via J13,J28&J29connector |
Signals Brought out via J14 connector |
|
|
PRUSS |
NIL |
NIL |
|
|
Expansion Connectors |
J13,J128&J29 |
J14 &J15 |
|
|
|
|
|
|
|
Power Supply |
PMIC –control through I2C and measure power on the individual rails |
Fixed Voltage Regulator |
|
|
|
|
|
|
|
Boot Modes Support |
|
|
|
|
|
|
|
|
|
Debug |
|
|
LCDK -(No onboard emulator; external emulator is required)
|
|
|
|
|
|
|
Software |
|
|
|
|
DSP/BIOS |
|
|
|
|
Starter Ware/Examples |
Board Support Library (BSL) sample programs to test the Logic –PD EMV board’s |
LCDK include Starter ware Support http://www.ti.com/tool/starterware-dsparm |
Some of the Logic PD sample program can be executed in LCDK .Starter remains the same for both the platform |
|
Linux SDK & U-boot |
Logic PD Linux Demo and U-boot (Boot loader/Monitor) |
Includes TI Linux demo ,U-Boot & SDK |
|
Note:
For Logic PD 4.3” WQVGA LCD
Development Kit includes a 4.3" WQVGA LCD with a 4-wire touchscreen
Integrated LCD, touch, and backlight connector for optional Zoom Display Kits
OMAP-L138 EVM UI Board
Some addition features are present in the OMAP-L138 EVM UI interface board vs. LCDK board differences outlined below
|
OMAP-L138 UI board |
LCDK |
|
|
|
Video
|
S-video in/out connector (TVP5147/ADV7343) Camera interface
|
NIL |
Feature not present in LCDK board |
|
Analog video in/out connectors (TVP5147/ADV7343)
|
Analog video IN (Composite IN) (TVP5147M1PFP) |
|
|
|
Analog to digital converter (ADS901)
|
NIL |
Feature not present in LCDK board |
|
|
Digital to analog converter (DAC900)
|
Video DAC (THS8135) VGA out through 15 pin D-SUB |
|
|
|
Camera interface |
On board connector for One Leopard Imaging Camera Sensor Input (36-pin ZIP connector)
|
|
|
|
LCD Panel |
48-character LCD panel |
NIL |
Only (Beagleboard XM connectors) for LCD interface in LCDK board |
|
Network Support |
One RJ45 Ethernet jack connector |
On board RJ45 Connector with magnetics and status LED’s |
|
|
Memory |
+ 8 MB NOR flash + 512 MB NAND flash |
On board
|
|
Regards
Antony
Hi,
one thing which could be a problem for someone is that the Logic PD OMAP-L138 Experimenter Kit has all important pins like GPIO, SPI, I2C, McASP, McBSP, I2S on Hirose 0.4mm pitch connectors only.
So actually only ADC and DAC Audio IN/OUT is available.
And I haven't found any information about the UI board (price/availability), so there is probably no chance to buy it separately.
Regards,
Jiri